cancel
Showing results for 
Search instead for 
Did you mean: 

Confusion of temperature calibration points used in production for STM32G474

KaiyangChu
Associate

Refer to datasheet DS12288 Rev 6(STM32G474xB STM32G474xC STM32G474xE), where Table 5 (Temperature sensor calibration values) describes that the high temperature calibration sampling point used for internal temperature sensor calibration is 130 degrees Celsius, but in the LL library, 110 degrees Celsius is used for temperature conversion.

KaiyangChu_0-1737563568647.png

stm32g4xx_ll_adc.h: line 386

 

#define TEMPSENSOR_CAL2_TEMP               (110L)                       /* Temperature at which temperature sensor
                                           has been calibrated in production for data into TEMPSENSOR_CAL2_ADDR
                                           (tolerance: +-5 DegC) (unit: DegC). */

 

Which one is correct?

1 ACCEPTED SOLUTION

Accepted Solutions
Igor Cesko
ST Employee

Hello KaiyangChu,

 Please use new version of drivers - where this was corrected to correct value (130°C).

 

  Regards

                         Igor

View solution in original post

1 REPLY 1
Igor Cesko
ST Employee

Hello KaiyangChu,

 Please use new version of drivers - where this was corrected to correct value (130°C).

 

  Regards

                         Igor