2017-12-30 06:30 AM
Hello together,
I try to make my first, baby steps with cortex controller.
Currently I try to set up an USART and using the free edition of uVision 5. When I try to compile my code I get about 2*30erros out of stm32l4xx_ll_usart.h (which I had copied in my project folder.) which are always the both below:
_STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *
SARTx)_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(649): error: #90: function returning function is not allowed_STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *SARTx)_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(649): error: #141-D: unnamed prototyped parameters not allowed when body is present __STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *USARTx)_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(660): error: #79: expected a type specifierDoes someone has any ideas? I also try to compile a project out of the example folders. This works fine without any erros (exapt that I cant recieve any information via usart in my terminal. Maybe the lib doesent work correct? But that is an other problem for a new thread ...). So I try to check and copy the project setting. But without success, unfortunately. Still about 60 compiler erros...
Solved! Go to Solution.
2018-01-04 04:24 AM
I don't know, what I have done (maybe cleaning the project, delete the files and add it new to the project). But the errors are gone now... Don't know ..
2018-01-04 04:24 AM
I don't know, what I have done (maybe cleaning the project, delete the files and add it new to the project). But the errors are gone now... Don't know ..