cancel
Showing results for 
Search instead for 
Did you mean: 

compiler errors out of stm32l4xx_ll_usart.h and stm32l4xx_ll_rcc.h

Marco Israel
Associate II
Posted on December 30, 2017 at 17:56

Hello,

I try to make my first baybesteps in arm cortex M. I use the free version of uVision 5. Currently I try to set up an USART. When I try to compile, I get the both erros below about 2*30 times out of stm32l4xx_ll_usart.h and stm32l4xx_ll_rcc.h:

_STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *

SARTx)

_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(649): error: #90: function returning function is not allowed

_STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *

SARTx)

_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(649): error: #141-D: unnamed prototyped parameters not allowed when body is present

__STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *USARTx)

_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(660): error: #79: expected a type specifier

I try to compile one usart example without any erros. So I checked and copied the project settings. but without any new result. Still errors.

Does someone has any idea which helps me to fix my mistake?

Kind regards

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Marco Israel
Associate II
Posted on January 04, 2018 at 13:23

I don't know, what I have done (maybe cleaning the project, delete the files and add it new to the project). But the errors are gone now... Don't know ..  

View solution in original post

1 REPLY 1
Marco Israel
Associate II
Posted on January 04, 2018 at 13:23

I don't know, what I have done (maybe cleaning the project, delete the files and add it new to the project). But the errors are gone now... Don't know ..