2017-07-12 4:35 AM
the LL library of the stm32f4xx and stm32f7xx , is the same ?
2017-07-12 5:14 AM
Hello
youssef.elmzaiti
,To see more about Low layer drivers on STM32F7 and STM32F4, refer to the user manual:
With Regards
Imen
2017-07-14 1:24 AM
Hello
youssef.elmzaiti
,LL libraries are designed for very low-level tasks and there is general compatibility between them, but this is not the case for all peripherals. There can be incompatibility and some functions which exists in F7, are not available on F4, depends on device features, and vice-versa of course.
2017-07-19 8:49 AM
,
,
2017-07-14 10:24 GMT+02:00 Tilen MAJERLE <,st-microelectronics@jiveon.com>,:
STMicroelectronics Community
<,https://community.st.com/?et=notification.mention>,
You have been mentioned
by Tilen MAJERLE
<,
Re: compatibility between LL library of stm32f4 and stm32f7 in
STMicroelectronics Community* - View Tilen MAJERLE's reference to you
<,https://community.st.com/0D70X000006Sp8aSAC