cancel
Showing results for 
Search instead for 
Did you mean: 

How to port the MIPI camera with STM32F4?

chrishs1027
Associate II
Posted on December 23, 2015 at 02:42

Dear all.

We have a project to calculate the optical flow by STM32F427.

Like the following project : https://pixhawk.org/modules/px4flow

But we chose the camera OV7251 instead of MT9V034.

The main problem is the interface of the OV7251 is MIPI CSI2.

So we added the bridge IC STMIPID02 to convert the signal between MIPI and parallel in order to send the image to the STM32F427.

But I am not sure is the design is reasonable? (MIPI camera + STMIPID02 + STM32F427)

Had anyone designed the MIPI camera with STM32F4?

Appreciate for any information.

#stm32f4-mipi
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Posted on December 23, 2015 at 14:16

Not sure there is a very deep level of camera/DCMI experience on the forum.

Skimming the data sheets my immediate concern would be the 1.8V levels on the parallel interface.

You probably want to evaluate your camera/interface choices on a dev board presenting a DCMI interface, and building a proto-type.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
chrishs1027
Associate II
Posted on December 24, 2015 at 06:40

Hi Clive1.

Thanks for your response.

We had added the level translator to shift the voltage between 1.8V and 3.3V.

But we really want to know how to integrate the MIPI camera with STM32F4.

And if the design is reasonable ?(MIPI camera + STMIPID02 + STM32F427)

Regards

Chris

Posted on December 24, 2015 at 16:28

It doesn't seem unreasonable, but the devil will be in the detail, and all the configuration, clocks and bandwidth. The size of the frame buffer, and the limits of the STM32 DMA controller will also likely play a role.

I'm really not getting a good sense of whether you are bringing any prior experience with any of the technology/concepts involved here. Do you have a complete working understanding of the other project you cited here?

For a corporate customer, your best approach would be via the ST sales and distribution offices, an access to an FAE with experience in the camera integration area. You might also want to review the list of contractors and consultants for those with camera experience.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
megahercas6
Senior
Posted on December 24, 2015 at 23:05

MIPI is supported only by STM32F479 or STM32F469 ( have hardware for it)

chrishs1027
Associate II
Posted on December 25, 2015 at 02:44

Hi Linas.

I had surveyed the specification of the STM32F479 and STM32F469.

But they only support MIPI-DSI display interfaces not the MIPI-CSI camera interface.

So I didn't choose the STM32F479 or STM32F469 as the MCU.

Posted on January 06, 2017 at 05:41

Hi  chris,have you solved the problem ? I meet the same problem ,too.

I have an idea,don't know whether it works.

As you say ,STM32F469  support MIPI-DSI,can we use the PHY  STM32F469 serve for DSI,  do with CSI.?

(would you like to paeden my poor english)

Nikita Polupanov
Associate
Posted on July 19, 2017 at 18:08

Hello!

Have someone solved this problem? I want to use STMIPID02 to connect camera to STM32F767 chip. I'd appreciate any help.

sincerely