cancel
Showing results for 
Search instead for 
Did you mean: 

Communication between two stm32l031k6 (lib STM32cubemx)

ibrahim
Associate II
Posted on July 07, 2016 at 10:50

Hello xD,

I want to communicate with two STM32L031K6 in SPI with the library HAL for STM32CubeMX.

I configure a Master with emission interruption and the other in slave reception with interruption. and I connect the two STM32 with son

(PA5) MOSI --- (PA5)MOSI,

(PB4)MISO--- MISO

(PB5) SCK --- SCK.

But I can not communicate or to receive the data. I do not know why. That is my program. Thank you very much.

spi.c

/* Includes ------------------------------------------------------------------*/

#include ''spi.h''

#include ''gpio.h''

extern __IO uint8_t data_get[1];

SPI_HandleTypeDef hspi1;

/* SPI1 init function */

void MX_SPI1_Init(void)

{

hspi1.Instance = SPI1;

/* master mode for stm32 send data */

hspi1.Init.Mode = SPI_MODE_MASTER;

/* slave mode for stm32 receive data */

//hspi1.Init.Mode = SPI_MODE_SLAVE;

hspi1.Init.Direction = SPI_DIRECTION_2LINES;

hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;

hspi1.Init.NSS = SPI_NSS_SOFT;

hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;

hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

hspi1.Init.CRCPolynomial = 7;

if (HAL_SPI_Init(&hspi1) != HAL_OK)

{

Error_Handler();

}

}

void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)

{

GPIO_InitTypeDef GPIO_InitStruct;

if(spiHandle->Instance==SPI1)

{

/* Peripheral clock enable */

__HAL_RCC_SPI1_CLK_ENABLE();

/**SPI1 GPIO Configuration

PA5 ------> SPI1_SCK

PB4 ------> SPI1_MISO

PB5 ------> SPI1_MOSI

*/

GPIO_InitStruct.Pin = GPIO_PIN_5;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

GPIO_InitStruct.Alternate = GPIO_AF0_SPI1;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

GPIO_InitStruct.Alternate = GPIO_AF0_SPI1;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

}

}

void HAL_SPI_MspDeInit(SPI_HandleTypeDef* spiHandle)

{

if(spiHandle->Instance==SPI1)

{

/* Peripheral clock disable */

__HAL_RCC_SPI1_CLK_DISABLE();

/**SPI1 GPIO Configuration

PA5 ------> SPI1_SCK

PB4 ------> SPI1_MISO

PB5 ------> SPI1_MOSI

*/

HAL_GPIO_DeInit(GPIOA, GPIO_PIN_5);

HAL_GPIO_DeInit(GPIOB, GPIO_PIN_4|GPIO_PIN_5);

}

}

main.c

/* Includes ------------------------------------------------------------------*/

#include ''stm32l0xx_hal.h''

#include <..\MDK-ARM\Hardware.h>

#include ''usart.h''

#include ''gpio.h''

#include ''tim.h''

#include ''spi.h''

#define BUFFERSIZE 100

volatile uint8_t data_get[1];

volatile uint8_t Save_data[1];

volatile int Index_BufferRx_SPI = 0;

int count_data = 0;

volatile uint8_t SPIStatus;

volatile uint8_t aTxBuffer[BUFFERSIZE] = ''SPI Master/Slave : Communication between two SPI using Interrupts'';

volatile uint8_t aRxbuffer[BUFFERSIZE];

int main(void)

{

/* initialization UART, SPI, TIMER and GPIO */

HW_Init();

#if 0

/* Enable flag interrupt emission */

__HAL_SPI_ENABLE_IT(&hspi1, (SPI_IT_TXE));

HAL_SPI_Transmit_IT(&hspi1, (uint8_t *) aTxBuffer, 100);

#endif

#if 1

/* Enable flag interrupt recption */

__HAL_SPI_ENABLE_IT(&hspi1, (SPI_IT_RXNE));

HAL_SPI_Receive_IT(&hspi1, (uint8_t *) data_get, 1);

#endif

while(1)

{

}

}

void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)

{

if(hspi->Instance == hspi1.Instance)

{

/* Save data and filling the table aRxbuffer */

Save_data[0] = data_get[0];

aRxbuffer[Index_BufferRx_SPI] = Save_data[0];

Index_BufferRx_SPI++;

}

/* it's ok to receive anathor data */

SPIStatus = HAL_SPI_Receive_IT(&hspi1, (uint8_t *) data_get, 1);

while(SPIStatus != HAL_OK)

{

HAL_SPI_Receive_IT(&hspi1, (uint8_t *) data_get, 1);

}

Index_BufferRx_SPI = 0;

}

void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi)

{

if(hspi->Instance == hspi1.Instance)

{

SPIStatus = HAL_SPI_Transmit_IT(&hspi1, (uint8_t *) aTxBuffer, 100);

while(SPIStatus != HAL_OK)

{

HAL_SPI_Transmit_IT(&hspi1, (uint8_t *) aTxBuffer, 100);

}

}

}

 

#stm32 #spi #stm32l0

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
serg2
Associate
Posted on July 08, 2016 at 09:49

-removed.