Communication between two stm32l031k6 (lib STM32cubemx)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-07-07 1:50 AM
Hello xD,
I want to communicate with two STM32L031K6 in SPI with the library HAL for STM32CubeMX. I configure a Master with emission interruption and the other in slave reception with interruption. and I connect the two STM32 with son (PA5) MOSI --- (PA5)MOSI, (PB4)MISO--- MISO (PB5) SCK --- SCK. But I can not communicate or to receive the data. I do not know why. That is my program. Thank you very much. spi.c/* Includes ------------------------------------------------------------------*/
#include ''spi.h'' #include ''gpio.h'' extern __IO uint8_t data_get[1]; SPI_HandleTypeDef hspi1; /* SPI1 init function */ void MX_SPI1_Init(void) { hspi1.Instance = SPI1; /* master mode for stm32 send data */ hspi1.Init.Mode = SPI_MODE_MASTER; /* slave mode for stm32 receive data */ //hspi1.Init.Mode = SPI_MODE_SLAVE; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 7; if (HAL_SPI_Init(&hspi1) != HAL_OK) { Error_Handler(); } } void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle) { GPIO_InitTypeDef GPIO_InitStruct; if(spiHandle->Instance==SPI1) { /* Peripheral clock enable */ __HAL_RCC_SPI1_CLK_ENABLE(); /**SPI1 GPIO Configuration PA5 ------> SPI1_SCK PB4 ------> SPI1_MISO PB5 ------> SPI1_MOSI */ GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF0_SPI1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF0_SPI1; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); } } void HAL_SPI_MspDeInit(SPI_HandleTypeDef* spiHandle) { if(spiHandle->Instance==SPI1) { /* Peripheral clock disable */ __HAL_RCC_SPI1_CLK_DISABLE(); /**SPI1 GPIO Configuration PA5 ------> SPI1_SCK PB4 ------> SPI1_MISO PB5 ------> SPI1_MOSI */ HAL_GPIO_DeInit(GPIOA, GPIO_PIN_5); HAL_GPIO_DeInit(GPIOB, GPIO_PIN_4|GPIO_PIN_5); } } main.c/* Includes ------------------------------------------------------------------*/
#include ''stm32l0xx_hal.h''
#include <..\MDK-ARM\Hardware.h>
#include ''usart.h''
#include ''gpio.h''
#include ''tim.h''
#include ''spi.h''
#define BUFFERSIZE 100
volatile uint8_t data_get[1];
volatile uint8_t Save_data[1];
volatile int Index_BufferRx_SPI = 0;
int count_data = 0;
volatile uint8_t SPIStatus;
volatile uint8_t aTxBuffer[BUFFERSIZE] = ''SPI Master/Slave : Communication between two SPI using Interrupts'';
volatile uint8_t aRxbuffer[BUFFERSIZE];
int main(void)
{
/* initialization UART, SPI, TIMER and GPIO */
HW_Init();
#if 0
/* Enable flag interrupt emission */
__HAL_SPI_ENABLE_IT(&hspi1, (SPI_IT_TXE));
HAL_SPI_Transmit_IT(&hspi1, (uint8_t *) aTxBuffer, 100);
#endif
#if 1
/* Enable flag interrupt recption */
__HAL_SPI_ENABLE_IT(&hspi1, (SPI_IT_RXNE));
HAL_SPI_Receive_IT(&hspi1, (uint8_t *) data_get, 1);
#endif
while(1)
{
}
}
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
if(hspi->Instance == hspi1.Instance)
{
/* Save data and filling the table aRxbuffer */
Save_data[0] = data_get[0];
aRxbuffer[Index_BufferRx_SPI] = Save_data[0];
Index_BufferRx_SPI++;
}
/* it's ok to receive anathor data */
SPIStatus = HAL_SPI_Receive_IT(&hspi1, (uint8_t *) data_get, 1);
while(SPIStatus != HAL_OK)
{
HAL_SPI_Receive_IT(&hspi1, (uint8_t *) data_get, 1);
}
Index_BufferRx_SPI = 0;
}
void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi)
{
if(hspi->Instance == hspi1.Instance)
{
SPIStatus = HAL_SPI_Transmit_IT(&hspi1, (uint8_t *) aTxBuffer, 100);
while(SPIStatus != HAL_OK)
{
HAL_SPI_Transmit_IT(&hspi1, (uint8_t *) aTxBuffer, 100);
}
}
}
#stm32 #spi #stm32l0
- Labels:
-
SPI
-
STM32L0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-07-08 12:49 AM
-removed.