Skip to main content
remae
Associate
July 7, 2016
Question

A CUBE issue: float mode from hard to ''soft'' with no explanation

  • July 7, 2016
  • 2 replies
  • 726 views
Posted on July 07, 2016 at 15:04

Hi,

i have a problem with CUBE and System Workbench.

Each time i click the ''Generate code'' the FPU mode in Drivers and/or Middlewares is randomly switched from hard to soft (--abi-float=soft)

The code won't compile then.

It's very annoying because this behavior is very random: sometimes only the Drivers branch is touched, sometimes both Drivers and Middlewares are changed.

Is my problem unique or there's a solution for a ''permanent'' float setting in Eclipse?

I need ''hard''.

-

Using the System Workshop Luna Release 2 (4.4.2) and Cube MX 4.14.0 on Windows.
    This topic has been closed for replies.

    2 replies

    Radosław
    Associate II
    July 7, 2016
    Posted on July 07, 2016 at 19:34

    If STemwin is in use, then softfpu is required.

    soft fpu still use FPU but calling is different.

    remae
    remaeAuthor
    Associate
    July 8, 2016
    Posted on July 08, 2016 at 11:09

    Okay, but it silently changes also the Driver's MPU to ''-mthumb''. The rest of project remains unchanged. You can easily imagine what happens then, on execution.

    THE PROBLEM IS:

    After each of code generations the Drivers MPU Setting is not more inherited from  the project root, and in 50% of the cases Drivers in plus are completely excluded from the build.

    I can re-include Drivers back but I cannot change the Drivers MPU settings to anything - nor hard, nor softp.

    The only way to ''fix'' it is to delete the entire Drivers folder physically and to copy it back.