2024-03-14 4:26 AM
Dear all,
is it possible to use CMSIS-DSP with STM32F302XXX?
Actually I'm working with NUCLEO STM32F302R8Tx (but final board will have STM32F302RCT6) and I have two issues :
1) I am not able to find lib *.a in repository CMSIS_DSP
2) Following this guide Guide I get this error ../Drivers/CMSIS/Include/core_cm4.h:105:8: error: #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
Is there some hardware limitation?
Or am I missing some step?
Thank you
Solved! Go to Solution.
2024-03-14 4:35 AM - edited 2024-03-14 4:36 AM
@ermes wrote:2) Following this guide Guide I get this error ../Drivers/CMSIS/Include/core_cm4.h:105:8: error: #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
Well, the STM32F302R8 does have an FPU - so there must be a problem in your configuration:
Have you tried a search of the forum?
2024-03-14 4:35 AM - edited 2024-03-14 4:36 AM
@ermes wrote:2) Following this guide Guide I get this error ../Drivers/CMSIS/Include/core_cm4.h:105:8: error: #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
Well, the STM32F302R8 does have an FPU - so there must be a problem in your configuration:
Have you tried a search of the forum?
2024-03-14 4:59 AM
Hello,
As stated by @Andrew Neil STM32F302 has a HW FPU.
Check out the DSP demo provided in X-CUBE-DSPDEMO (STM32F429I-Discovery project) which you can inspire from.