cancel
Showing results for 
Search instead for 
Did you mean: 

CAN2 does not send or receive message in nomal mode

Apo
Associate

Hi,

I am trying to set up a project with 2 can buses (CAN1 and CAN2), 

First goal was to check if both CAN1 and CAN2 would be able to receive and send messages. 

I read a bit about people struggling to make both can work because of the "master-slave" can filter configuration that was not clearly explained in the reference manual especially when setting the can filterbank "cursor". Therefore I took care of CAN's filter configuration and my MX_CAN1_Init and MX_CAN2_Init looks like this:

/**
* @brief CAN1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_CAN1_Init(void)
{

/* USER CODE BEGIN CAN1_Init 0 */

/* USER CODE END CAN1_Init 0 */

/* USER CODE BEGIN CAN1_Init 1 */

/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 4;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_2TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = ENABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
CAN_FilterTypeDef sFilterConfig;
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 14;
if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
HAL_CAN_Start(&hcan1);

if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
/* Notification Error */
Error_Handler();
}
/* USER CODE END CAN1_Init 2 */

}

/**
* @brief CAN2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_CAN2_Init(void)
{

/* USER CODE BEGIN CAN2_Init 0 */

/* USER CODE END CAN2_Init 0 */

/* USER CODE BEGIN CAN2_Init 1 */

/* USER CODE END CAN2_Init 1 */
hcan2.Instance = CAN2;
hcan2.Init.Prescaler = 4;
hcan2.Init.Mode = CAN_MODE_NORMAL;
hcan2.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan2.Init.TimeSeg1 = CAN_BS1_2TQ;
hcan2.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan2.Init.TimeTriggeredMode = DISABLE;
hcan2.Init.AutoBusOff = DISABLE;
hcan2.Init.AutoWakeUp = DISABLE;
hcan2.Init.AutoRetransmission = ENABLE;
hcan2.Init.ReceiveFifoLocked = DISABLE;
hcan2.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN2_Init 2 */
CAN_FilterTypeDef sFilterConfig;
sFilterConfig.FilterBank = 14;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 14;
if (HAL_CAN_ConfigFilter(&hcan2, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}

HAL_CAN_Start(&hcan2);

/*##-4- Activate CAN RX notification #######################################*/
if (HAL_CAN_ActivateNotification(&hcan2, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
/* Notification Error */
Error_Handler();
}
/* USER CODE END CAN2_Init 2 */

}

I've also activated both can RX0 interrupt and declared the HAL_CAN_RxFifo0MsgPendingCallback inside my main.c file. 

Both can buses are connected to a PEAK CAN-USB interface in order to check traffic on each bus. 

First test was done with CAN1 in normal mode and CAN2 in loopback silentmode. This test went well as I saw in debugging mode that CAN2 messages were successfully sent and that the CAN_RxfifoMsgPendingCallback was fired. 

Second test was done with both CAN1 and CAN2 in normal mode. I was expecting seeing a CAN2 message coming out using my can-usb monitor. However, no messages came out, the CAN2 mailboxes were filled until 3d level and then an error occured due to full CAN2 transmit mailboxes (HAL_CAN_ERROR_PARAM)

I've tried to check both CAN2 pins on an oscilloscope and I got no signal..

Same problem occured with the CAN2 reception while sending messages using the CAN-USB to send a message towards CAN2. 

To sum up, while I have no problem with CAN1 transmission and reception, I got serious difficulties making CAN2 work without this strange behavior. 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
mÆŽALLEm
ST Employee

Also Check the state of the transceiver connected to CAN2.

Some transceivers have standby mode/enable pin. So if the transceiver is disabled you cannot establish CAN communication

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mÆŽALLEm
ST Employee

Hello,

First check the following:

- Pin used for CAN2_Tx and CAN2_Rx . 

- Their configs

- Check their connections to the transceiver

I suspect something in the pins selection (are they the ones connected to the CAN transceiver?) or their config

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mÆŽALLEm
ST Employee

Also Check the state of the transceiver connected to CAN2.

Some transceivers have standby mode/enable pin. So if the transceiver is disabled you cannot establish CAN communication

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thanks for you prompt response. 

Actually Cmy transceiver does not have standby mode/enable pin. Anyway, I've checked my transceiver datasheet and saw that a red jumper was used to activate the "end line" 120 ohm resistor. As my differential line was ridiculously short (from the transceiver output to the CAN-USB input), I removed the jumper and that's when I started seing can correct messages coming out of CAN2.

Communication established ! 

Thanks for your support,