2025-02-25 10:52 PM
Can the STM32N6 be connected to a 12MP image sensor for use solely in taking photos?
In Section 3.25 of the datasheet, it is mentioned:
"The DCMIPP path offers the following summarized maximum features:
• Target sensors: 5 MPixel at 30 fps max"
AND
"Some over-target use cases are possible, but with specific constraints:
• sensors with resolution above 5 Mpixels
• sensors with pixel rate above 150 Mpixel/s
• double sensors in parallel"
I know that STM32N6 can only support video of 5MP@ 30fps. However, if I only use it for taking still images, can the input pixel resolution be greater than 5 MP?Like 12MP (IMX681)
In Section 3.31 of the datasheet, it is mentioned:
" Still-image encode:
– codecs: JPEG (baseline interleaved)
– performance: 300 Mpixel/s for JPEG"
From my understanding, from the VENC perspective, it should be able to support higher pixel resolutions for still images as well. However, there is no explicit mention of this in the datasheet. Could everyone please help clarify my doubt?