cancel
Showing results for 
Search instead for 
Did you mean: 

Can the ADCs on the STM32F767 be configured in differential input mode?

MPicc
Associate II

In some of the tutorial materials it mentions that the ADCs on the STM32F7 devices can be used in single-ended or differential input modes. I have studied the reference manual but have had no luck in defining how to use the STM32F767's ADC in differential input mode. Am I missing something, and if so can someone point me in the right direction towards accomplishing differential input mode on this device.

Thanks in advance!

2 REPLIES 2

> In some of the tutorial materials

Namely?

AFAIK, differential mode is on only in ADC of 'F3, 'L4 and 'H7 (probably also the new 'G4, I did not check that).

JW

MPicc
Associate II

Mentioned in link below on "STM32F7 Online Training" slide 3. Thanks for the clarification.

https://st-onlinetraining.s3.amazonaws.com/STM32F7-Analog_ADC/index.html