Can't get expected results working with external memory with I2C
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-09 07:59 PM
Hello people from ST community,
I'm here today talking about I2C, starting to working on it and wanted to see if I could fix an issue telling you my experience with an external EERAM memory, the 47L16 EERAM from Microchip. My board is a Nucleo F411RE
I am currently able to talk to the device according to my code output and previous testing. But I am trying to doing a write a byte to the SRAM (0x22) and then read it back from the same memory address but and I am unable to get to work properly, I always get 0xFF as response in my UART output prints...
in HAL_I2C_Mem_Read() function, is the 5th parameter (pData, pointer to the data buffer) the data buffer that will hold the response from the slave devices (EERAM memory)? What should I do in order to do this process?
I think I am missing something important to get this properly working. Thank you so much in advance for any incoming ideas.
// EERAM Tasks
// write to the 0x10 register
uint8_t buf[15] = {0}; // buffer to print data at the end
uint8_t pdata[1] = {0x22}; // write in the SRAM
uint8_t output[1] = {0}; // store value read from SRAM
const uint16_t ADDR_WRITE = 0xA0; // device slave address to write
const uint16_t ADDR_MEMORY = 0x10; // memory address to write to
// write 0x22 to the SRAM
ret = HAL_I2C_Mem_Write(&hi2c1, ADDR_WRITE, ADDR_MEMORY, 1, pdata, 1, HAL_MAX_DELAY);
if(ret != HAL_OK) {
DebugStringOut(&huart2, "Error Tx 1\r\n");
}
else {
// read 0x22 from SRAM
const uint16_t ADDR_READ = 0xA1; // device slave address to read
ret = HAL_I2C_Mem_Read(&hi2c1, ADDR_READ, ADDR_MEMORY, 1, output, 1, HAL_MAX_DELAY);
if(ret != HAL_OK) {
DebugStringOut(&huart2, "Error Rx\r\n");
}
else {
sprintf((char*)buf, "rx->%d\r\n", output[0]);
DebugStringOut(&huart2, (char*)buf);
}
}
- Labels:
-
I2C
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-10 05:10 AM
/**
* @brief Write an amount of data in blocking mode to a specific memory address
* @param hi2c Pointer to a I2C_HandleTypeDef structure that contains
* the configuration information for the specified I2C.
* @param DevAddress Target device address: The device 7 bits address value
* in datasheet must be shifted to the left before calling the interface
* @param MemAddress Internal memory address
* @param MemAddSize Size of internal memory address
* @param pData Pointer to data buffer
* @param Size Amount of data to be sent
* @param Timeout Timeout duration
* @retval HAL status
*/
HAL_StatusTypeDef HAL_I2C_Mem_Write(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress, uint16_t MemAddSize, uint8_t *pData, uint16_t Size, uint32_t Timeout)
{
Your 4th parameter is incorrect. The device wants a 16 bit address. So send MemAddress=I2C_MEMADD_SIZE_16BIT.
You don't need to pass 0xA1 to write. The software will add the trailing bit for you. You can just pass 0x40.