cancel
Showing results for 
Search instead for 
Did you mean: 

Can STM32H7 DAC DMA work without a trigger, and instead use DMAMUX synchronization?

Andrew Sterian
Associate III

The documentation for the DAC says "A DMA request can be generated when an external trigger (but not a software trigger) occurs if DMA requests are enabled"

But I want to configure the DAC to have no trigger, and instead use TIM12_TRGO to drive the DAC conversion pace, using it as a DMAMUX synchronization input.

Will this work? Or do I absolutely need to configure the DAC with an external trigger to use DMA?

3 REPLIES 3
jiangfan
ST Employee

it is not clear which STM32H7 you use.

it is possible to use Timer to trigger DAC conversion.

According to RM0468 Reference manual, STM32H723/733, STM32H725/735 and STM32H730 Value line. DAC conversion may be triggered by TIM1/2, TIM4~8, TIM15 and so on. DAC conversion may also be triggered by external pin: exti9.

0693W00000FC1fiQAD.gif

Andrew Sterian
Associate III

It is the STM32H725, but DAC conversion can also be triggered by simply writing to the DAC_DHRx if the TENx bit is 0 (i.e., no trigger).

So my question is, in this case (TENx=0), can the pace of the DAC writes be driven by DMAMUX synchronization?

jiangfan
ST Employee

I suppose, the idea is, to use Timer (such as TIM12) to trigger DMA transfer automatically in a desired period, the DMA will perform transfer from memory (data buffer) to DAC data holding register (such as DAC_DHR12R1), and DAC output is updated in very short time with TEN1=0 (data written into the DAC_DHR1 register are transferred one dac_pclk clock cycle later to the DAC_DOR1 register).

I think this should work.