2019-06-05 05:41 PM
2019-06-05 05:46 PM
Using FSMC and FPGA you'd could presumably interface it to anything you can describe in VHDL or VERILOG
2019-06-05 05:47 PM
Some cards use power and USB
2019-06-06 12:45 AM
PLX (acquired by Avago, which goes under Broadcom name this week) produces PCIe-to-parallel-bus bridges, see PEX8311.
What is TPU?
JW
2019-06-06 01:04 AM
I would guess the "Timing Processor Unit" of the Motorola 683xx family.
https://en.wikipedia.org/wiki/Freescale_683XX
Not sure if it would make sense to integrate it with a STM32F4.
2019-06-10 02:35 AM
google's tpu
2019-06-10 02:46 AM
but how to connect to stm32?