2025-01-21 1:55 PM
We did many projects using Stm32f105rbt6. Stm32f103ret6 now is cheaper with more memory and the pinout is the same. Can we use Stm32f103ret6 directly without any programming changes?
2025-01-21 2:27 PM
Dear @ax369 ,
The major difference is USB peripheral that is not compatible and should change the software and so some Clocks settings at system level . Then the migration is straightforward and easy between parts especially on the Flash and memories .
Hope it helps you.
STOne-32
2025-01-21 3:21 PM
Thank you. Can you please point me to where I can find exactly what to change to the software so that it’s compatible with both?