2025-01-21 12:22 AM
I down load the STM32F373C8T6 Foot print and Symbol from STs website (Ultalibrarian)
But it has a wrong Pinouts connections (Pin numbers)
VDD_2 Pin No.14
PA-4 Pin No 15
PA-5 Pin No 16
PA-6 Pin No 17
But actual connections are
PA-4. Pin No 14
PA-5. Pin No 15
PA-6. Pin No 16
VDD_2. Pin No 17
Please observe this anyone designing with this foot print , and
I Request ST to correct this foot print and Symbols
2025-01-21 2:46 PM - edited 2025-01-22 12:27 AM
Hello @vbakoti and welcome to the ST Community.
I confirm this typo and I've escalated to the concerned team for correction ASAP (under internal ticket number 201049).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.