Can someone explain the DMAMUX mapping on the STM32G431?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-11 8:18 PM
I read the ref manual several times but it is still unclear to me. I have a problem with a DMA design that is transferring TIM8_CH1 and TIM8_CH3 to memory using DMA_Channel1 and DMA_Channel2. I am getting a transfer error so am looking at what could cause this.
The timer value is uint32_t and the buffers are both 4-byte aligned. Is this okay? (I think so)
I do not understand the DMAMUX explanation in the ref manual page RM0440, page 384 Table 80. I see TIM8_CH1 is on DMA input request #49 and TIM8_CH3 is on DMA input request #51. How do these map to DMA Channel # on DMA1 and DMA2?
Can TIM8_CH1 and TIM8_CH3 be used respectively on DMA1_Channel1 and DMA1_Channel2. I can't seem to answer this from the ref manual do to my lack of understanding the explanation. The tables for the F303x and L41x are much clearer.
My understanding is a transfer error is caused by a bus fault, such as an illegal address. My destination data buffers are at 0x2000000C and 0x20000034. Are these an issue?
Thanks for any clarification you can offer, much appreciated.
BT
- Labels:
-
DMA
-
Documentation
-
STM32G4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-13 4:03 AM
Okay, I reduced my code to a minimum that was only running the DMA as described above. With TIM8 running and using capture on CH1 and CH3 I was able to trigger DMA1_CH1 and DMA2_CH2. Incidentally, this is using an external trigger on CH1 and a software trigger on CH3.
Whatever problem I am having in my complete code is not a problem with this Timer/DMA configuration. It still stands the DMAMUX documentation on the STM32G431 really fails compared to other ST devices. With 2127 pages in the Ref Manual they failed to communicate.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-03-10 7:07 AM
Hi @BTrem.1​ ,
A complementary content to what is already provided in the reference manual regarding DMA request multiplexer is provided in AN5224 (STM32 DMAMUX: the DMA request router).
Depending on the product where this multiplexer is available, this application note explains its features. It explains as well how to properly configure it.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.