2020-09-09 8:44 AM
I've been working with CAN on the STM32F1 for some time , but I'm having a terrible time trying to get it to work on the F303. I'm hoping someone can tell me what I'm doing wrong. Thanks very much for looking at it.
void can_gpio_config(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
//Configure CAN RX
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
//Configure CAN TX
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
//Connect pins
GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_7);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_7);
}
void can303_config(void)
{
CAN_InitTypeDef CAN_InitStructure;
CAN_FilterInitTypeDef CAN_FilterInitStructure;
can_gpio_config();
RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);
// CAN register init
CAN_DeInit(CAN1);
CAN_StructInit(&CAN_InitStructure);
CAN_InitStructure.CAN_TTCM = DISABLE;
CAN_InitStructure.CAN_ABOM = DISABLE;
CAN_InitStructure.CAN_AWUM = DISABLE;
CAN_InitStructure.CAN_NART = DISABLE;
CAN_InitStructure.CAN_RFLM = DISABLE;
CAN_InitStructure.CAN_TXFP = DISABLE;
CAN_InitStructure.CAN_Mode = CAN_Mode_Normal; //CAN_Mode_LoopBack; //CAN_Mode_Normal;
// Set the CAN Baudrate = 500K
//36,000,000 / (4 * (1 + 9 + 8)) =500,000
CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;
CAN_InitStructure.CAN_BS1 = CAN_BS1_9tq;
CAN_InitStructure.CAN_BS2 = CAN_BS2_8tq;
CAN_InitStructure.CAN_Prescaler = 4;
CAN_Init(CAN1, &CAN_InitStructure);
// CAN filter init
CAN_FilterInitStructure.CAN_FilterNumber = 0;
CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask;
CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_16bit;
CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000;
CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000;
CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0;
CAN_FilterInitStructure.CAN_FilterActivation = ENABLE;
CAN_FilterInit(&CAN_FilterInitStructure);
}Thanks again. I really appreciate it.
Solved! Go to Solution.
2020-09-09 9:03 AM
void can_gpio_config(void)
{
GPIO_InitTypeDef GPIO_InitStructure = {0};
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
//Configure CAN RX / TX
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11 | GPIO_Pin_12;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
//Connect pins
GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_9);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_9);
}
2020-09-09 9:03 AM
void can_gpio_config(void)
{
GPIO_InitTypeDef GPIO_InitStructure = {0};
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
//Configure CAN RX / TX
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11 | GPIO_Pin_12;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
//Connect pins
GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_9);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_9);
}
2020-09-09 1:05 PM
That did it. Thank you so much!