CAN Problem STM32F4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-03-30 4:09 AM
I'm having a hard time getting my STM32F4 discovery board to communicate with my CAN bus. I've successfully implemented a communication between CAN1 and CAN2 on the same Discovery Board, with a transceiver on each CAN port.
However, when I try to connect it to my CAN bus, I get HAL_TIMEOUT in the function HAL_CAN_Transmit();
I have dspic30f's that communicate flawlessly with my CAN bus, so I matched the STM32F4 Discovery bitrate to the pics, aswell as the relations between SJW, BS1 and BS2.
I'm only trying to transmit a CAN message, for the time being.
I've also tried to read the TX pin with a logic analyser. It detects the message but can't decode it properly.
Any help will be greatly appreciated.
Here's my code:
MX_GPIO_Init();
static
CanTxMsgTypeDef
TxMessage1;
static
CanRxMsgTypeDef
RxMessage1;/*♯♯-1- Configure the CAN peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
CanHandle1.
Instance
= CAN1;CanHandle1.
pTxMsg
= &TxMessage1;CanHandle1.
pRxMsg
= &RxMessage1;CAN_FilterConfTypeDef
sFilterConfig1;
/*♯♯-1- Configure the CAN peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
CanHandle1.
Init
.TTCM
=DISABLE
;CanHandle1.
Init
.ABOM
=DISABLE
;CanHandle1.
Init
.AWUM
=DISABLE
;CanHandle1.
Init
.NART
=DISABLE
;CanHandle1.
Init
.RFLM
=DISABLE
;CanHandle1.
Init
.TXFP
=DISABLE
;CanHandle1.
Init
.Mode
= CAN_MODE_NORMAL;CanHandle1.
Init
.SJW
= CAN_SJW_1TQ;CanHandle1.
Init
.BS1
= CAN_BS1_2TQ;CanHandle1.
Init
.BS2
= CAN_BS2_1TQ;CanHandle1.
Init
.Prescaler
= 11;
if
(HAL_CAN_Init(&CanHandle1) !=HAL_OK
){
/* Initialization Error */
Error_Handler();
}
/*♯♯-2- Configure the CAN Filter ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
sFilterConfig1.
FilterNumber
= 1;sFilterConfig1.
FilterMode
= CAN_FILTERMODE_IDMASK;sFilterConfig1.
FilterScale
= CAN_FILTERSCALE_32BIT;sFilterConfig1.
FilterIdHigh
= 0x0000;sFilterConfig1.
FilterIdLow
= 0x0000;sFilterConfig1.
FilterMaskIdHigh
= 0x0000;sFilterConfig1.
FilterMaskIdLow
= 0x0000;sFilterConfig1.
FilterFIFOAssignment
= 0;sFilterConfig1.
FilterActivation
= 1;sFilterConfig1.
BankNumber
= 0;
if
(HAL_CAN_ConfigFilter(&CanHandle1, &sFilterConfig1) !=HAL_OK
){
Error_Handler();
}
CanHandle1.
pTxMsg
->StdId
= 0x11;CanHandle1.
pTxMsg
->RTR
= CAN_RTR_DATA;CanHandle1.
pTxMsg
->IDE
= CAN_ID_STD;CanHandle1.
pTxMsg
->DLC
= 2;CanHandle1.
pTxMsg
->Data
[0] = 0xCA;CanHandle1.
pTxMsg
->Data
[1] = 0xFE;// Infinite loop
while
(1){
if
(HAL_CAN_Transmit(&CanHandle1, 10) !=HAL_OK
){
/* Transmission Error */
Error_Handler();
}
if
(HAL_CAN_GetState(&CanHandle1) !=HAL_CAN_STATE_READY
){
Error_Handler();
}
HAL_Delay(10);
}
}
#stm32f4-discovery #controller-area-network #can- Labels:
-
CAN
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-04-03 7:03 AM
It's working now. I had to match the exact time quantas of all the microcontrollers in the can bus.