cancel
Showing results for 
Search instead for 
Did you mean: 

CAN interface parameter settings

Bs.1
Associate II

Hi,

I am trying to implement CAN interface in STM32F072RBT6

System clock speed - 8MHz

Baud rate for CAN - 500Kbps

Prescalar - 1

CAN peripheral clock speed - 8 MHz

so TQ - 16

I have set the Time quanta seg1 - 9

Time quanta seg2 - 6

Time quanta sync width - 1

But I am not sure about how to set the seg1 & seg 2 values.

Can any one help me to clear this fundamentals, how to select these parameters?

1 ACCEPTED SOLUTION

Accepted Solutions
KnarfB
Principal III
2 REPLIES 2
KnarfB
Principal III

Hi...

Thanks for the reply