2020-12-16 3:54 PM
2020-12-17 9:54 AM
JW
2020-12-16 4:56 PM
Which STM32?
If 'F2/'F4, then answer to first question is yes.
JW
2020-12-17 3:10 AM
Hi VNado.1,
Best Regards,
Ons.
2020-12-17 7:43 AM
It is a L4+. I guess it also works?
2020-12-17 9:54 AM
JW
2020-12-17 2:29 PM
"Dual DAC channel independent or simultaneous conversions
• External triggers for conversion
The DAC channels are triggered through the timer update outputs that are also connected to different DMA channels."
2. I also saw this, but I wasn't sure if it was an error or something I was missing out.
Thanks!
2020-12-18 3:13 AM
Hi VNado.1,
In case your question is answered, please mark it by selecting the best answer.
Best Regards,
Ons.