cancel
Showing results for 
Search instead for 
Did you mean: 

SDRAM Chip Select & Clock Enable connections in STM32H750

Ahamed Faize
Associate II

Hi team,

We are using STM32H750 MCU in our design. We are interfacing an SDRAM memory to the MCU using FMC. But we have doubt on the SDRAM chip select & clock enable signals. We are planning to use FMC_SDNE0 & FMC_SDCKE0. But In Discovery kit, FMC_SDNE1 & FMC_SDCKE1 is used. So We have doubt such that Whether we should use the FMC_SDNE1 & FMC_SDCKE1 or whether we can use either 0 or 1, based on the pin availability?

Please clarify the above queries.

Regards,

Ahamed Faize

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

The two pairs of NE/CKE correspond to the two SDRAM banks, which are mapped to two address areas. Read the initial subchapters and SDRAM subchapter of FMC chapter in RM.

JW

Ahamed Faize
Associate II

Hi Jan,

Thanks.

I will go through the RM. I concluded from your answer is as below,

We can use either NE0/CKE0 or NE1/CKE1 if we are using single chip. But When we are using two chips, then NE0/CKE0 will be used for one device & NE1/CKE1 will be used for another device.

Just clarify me, Whether NE/CKE has to be used based on "No. of Banks" or "No. of Chips".

Regards,

Ahamed Faize