2021-05-14 2:49 AM
I am building an CAN system which includes sensor modules and actuator modules. There is 1 center MCU which control/communicate with all modules via can bus. I also want to update firmware for each module from that center MCU through CAN bus. Which hardware components i need for each module and is there any instruction or guide or example for doing that both hardware design and software design.
2021-05-14 3:33 AM
CAN is just a communication channel - of course you can use it to transfer your update data.
Having transferred the data, you will then have to program it into the microcontroller's flash - which is entirely independent of how you transported the data.
ST have several Application Notes on doing this; search for IAP - short for In-Application Programming ...
2021-05-16 8:09 PM
Thank you so much. "Program it into the microcontroller's flash" How can i do that. Can you explain me more about this. About the hardware design, do i need to put anymore component comparing to the normal build
2021-05-17 1:52 AM
Again: ST have several Application Notes on doing this; search for IAP - short for In-Application Programming ...