cancel
Showing results for 
Search instead for 
Did you mean: 

What is the meaning of each alphabet attached to the back of the nucleo board?

Lsang.1
Associate

For example, What does 'Z' and 'I' mean in Nucleo-F767ZI and what does 'Z' and 'G' mean in Nucleo-F767ZG?

In this way, please tell me the meaning of the things that are divided into R, E, B, K, C, etc.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

The Nucleo-F767ZI has an STM32F767ZI chip. The Z means it's an 144 pin package and the I means it has 2MB of FLASH. See the datasheet for specifics.

https://www.st.com/resource/en/datasheet/stm32f767zi.pdf

The Nucleo-F767ZG doesn't exist, but the NUCLEO-F746ZG has an STM32F746ZG chip. The G means it has 1MB of FLASH.

If you feel a post has answered your question, please click "Accept as Solution".
Mohamed Aymen HZAMI
ST Employee

Hello @Lsang.1​,

You can refer to the Ordering information section in datasheet , you will find all the information of each alphabet.

Mohamed Aymen.