2019-03-18 11:45 PM
hi dear.
I built a custom board based on the Stm32f796i-discovery Board.
I am trying to link TouchGFX but I can not write image to External Flash Memory (MX25L5124G).
The MX25L512G_STM32F769I-DISCO.stldr file is located in the External Loader folder of the ST-link utility.
I am sure someone will have an IAR Project for this file.
Can I get the IAR Project file for this file?
2020-08-07 7:25 AM
Hi ikassma,
I will woulk your request internally and see If I can come back with the the IAR Project you need for MX25L512G_STM32F769I-DISCO.stldr.
-Imen
2020-08-07 5:12 PM
thank you for your answer. if you can send iar project file at to my e mail address
2020-08-10 4:22 AM
Hi ikassma,
I did check for you and unfortunately I couldn't find the code source on IAR.
What I can suggest to you is to take a look at STM32F769 Firmware (here) under Drivers/BSP. You will find the QSPI drivers needed for the STM32F769I-Discovery board. You can include these files (.c/.h) in your project or just use the needed functions to perform actions to the External Flash Memory (write etc...)
I hope this help!
-Imen
2020-08-10 9:07 AM
It was written in Keil using the "F5" SPL, not likely something that's going to see the light of day..
Are you using different pins/clocks to the F769-DISCO ?
2020-08-11 1:37 AM
I actually solved this problem a year ago.
I solved the problem for about two weeks, and I wanted the project file because I wanted to compare it to the code I wrote.
I think ST's guidelines on how to program an external loader should be clearly documented. Please consider this.
To solve the problem a year ago, I solved it through various tests. I don't want anyone else to go through this trial and error.
2020-08-11 3:31 AM
Hi ikassma,
I believe the Drivers/BSP files should contain the needed steps to handle external memory (read, write etc...).
Nevertheless ST is in the process of placing Flash loader source codes on Github, I just don't have an official date on when it will become public for users.
Thank you for your feedbacks!
-Imen
2020-08-11 4:47 PM
Hi Imen.
The problem I encountered was that when the process of initializing was made as a single function and used, there was a symptom of freezing while trying to ERASE some pages of QSPI NOR FALSH.
I have been using it without any problems since I solved it one by one without making it a function.
I don't know why, but I think it was because I wasn't familiar with how to download and operate the code in the MCU's RAM. I think you will definitely need this.
thank you ^ㅡ^