2008-06-23 09:16 PM
Can I change STM32F103RB to 103RC with I2S on IAR 'KSDK-STM32-PLUS' ?
2011-05-17 03:37 AM
I wish to purchase and use the IAR kickstart for audio development using an I2S interface, so is it Ok to make a hardware change to the PCB and remove the STM32F103RB (which I believe only supports I2C), and replace it with the STMF103RC which has the I2S/I2C interface ?
Will the IAR 'KSDK-STM32-PLUS' software still work with the different chip ? I would be bery gratefull if sombody could advise me. Thanks Dave.