Skip to main content
Kneepatch
Senior
Feb 14, 2025 9:35 PM UTC
Solved

Can't Change GPIO Pull-up/Pull-down Mode for a Timer

I have a STM32F469I-DISCO board. It seems that I am unable to change the GPIO Pull-up/Pull-down Mode for a timer. I have tried to do it both in the CubeMX interface, and I have also looked through the HAL methods and attributes. I don't think it's an option. Does anyone happen to know why?

Kneepatch_0-1739568900354.png

 

This topic has been closed for replies.
Karl Yamashita
Karl YamashitaBest answer
Principal
Feb 14, 2025 11:14 PM UTC

It's at the bottom of the tab. Use the scroll bar

 

KarlYamashita_0-1739574805651.png

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source

3 replies

Karl Yamashita
Karl YamashitaBest answer
Principal
Feb 14, 2025 11:14 PM UTC

It's at the bottom of the tab. Use the scroll bar

 

KarlYamashita_0-1739574805651.png

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
TDK
Feb 14, 2025 11:17 PM UTC

After setting the pin as a TIMx pin, you can change the pullup/pulldown in the GPIO tab on the left side.

TDK_0-1739575063214.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Kneepatch
KneepatchAuthor
Senior
Feb 14, 2025 11:40 PM UTC

Oh my gosh, I totally missed scrolling down to see more options! I did check the GPIO part of the CubeMX, but again, I was blind and didn't see the TIM tab. Thanks everyone for the quick, thorough responses!

-Kneepatch