2018-03-19 2:24 AM
The __HAL_LOCK macro is defined as in stm32f1xx_hal_def.h
#define __HAL_LOCK(__HANDLE__) \
do{ \
if((__HANDLE__)->Lock == HAL_LOCKED) \
{ \
return HAL_BUSY; \
} \
else \
{ \
(__HANDLE__)->Lock = HAL_LOCKED; \
} \
}while (0)
So the Lock is read first and modified if needed. Would it cause race condition while the task calling __HAL_LOCK is preempted by a higher priority task which call __HAL_LOCK subsequently.
For example, task1 calls __HAL_LOCK and find the lock is open. task 1 is preempted by task2 whose priority is higher than task1 right before task1 write the Lock as HAL_LOCKED. task2 finds the lock is open and set the Lock as HAL_LOCKED. The task2 goes to block state to wait for some resource. Then task1 runs again and continue to get the lock. This will potentially corrupt the resources protect by the __HAL_LOCK for task2.
I would be happy if someone could correct me if I'm wrong since I could learn a lesson from it
2018-03-19 3:18 AM
Hi,
It seem to me, that your are right with multitasking. This code
__HAL_LOCK
is dangerous. It must be used from 1 task.If you want use in multitask like you, then need use critical sections (disable/enable interrupts) example (not tested).
#define __HAL_LOCK(__HANDLE__) \
do{ \
__disable_interrupts();
if((__HANDLE__)->Lock == HAL_LOCKED) \
{ \
/*
return HAL_BUSY; if we return, our task lost
*/ \__enable_interrupts(); /*let other task unlock */
\
Os_delay(1); /*let other task unlock */ \
} \
else \
{ \
(__HANDLE__)->Lock = HAL_LOCKED; \
__enable_interrupts(); /*let other task unlock */ \
break; \
} \
}while (1)
BR.
Darius Babrauskas
2018-03-19 5:03 AM
Thanks for the reply. What do you mean by 'if we return, our task lost'. The original __HAL_LOCK macro return HAL_BUSY if it is already locked by others. Shoudn't the thread safe version __HAL_LOCK follow the same regulation as the original one?
2018-03-19 5:17 AM
I mean, that we lost task (maybe better job). See code below from stm
if in HAL_ADC_Start __HAL_LOCK(hadc); return, then ADC not start measure.
HAL_StatusTypeDef HAL_ADC_Start(ADC_HandleTypeDef* hadc)
{ HAL_StatusTypeDef tmp_hal_status = HAL_OK; ADC_TypeDef *tmpADC_Master; /* Check the parameters */ assert_param(IS_ADC_ALL_INSTANCE(hadc->Instance)); /* Perform ADC enable and conversion start if no conversion is on going */ if (ADC_IS_CONVERSION_ONGOING_REGULAR(hadc) == RESET) { /* Process locked */ __HAL_LOCK(hadc);.............................
BR.
Darius Babrauskas
2018-03-19 8:21 PM
Yes, the task content will not get executed if __HAL_LOCK fails. But the caller can get this status from the return value and decide whether to delay and retry.
2018-03-20 1:24 AM
Yes you right, caller can get this status and decide whether to delay and retry. But her we have dangerous, because __HAL_LOCK can return incorrect condition or can execute protected code example:
&sharpdefine __HAL_LOCK(__HANDLE__) \
do{ \
if((__HANDLE__)->Lock == HAL_LOCKED) \
{ \
//other task switched her and unlock, so return not correct condition- it return busy, but it free!
return HAL_BUSY; \
} \
else \
{ \
//other task switched her and lock too, so 2 task use protected code (resource) !
(__HANDLE__)->Lock = HAL_LOCKED; \
} \
}while (0)
2018-05-14 8:21 AM
It's broken. See
for solutions.2018-05-14 12:21 PM
Thank you Morty.
I readed your link. But not sure that they are good solution.
My solution are tested by me more times and worked Ok.
BR.
Darius
2018-05-14 6:38 PM
another reason to never use multi tasking.
I find it best to process all state machines within a single foreground loop.
that way, there is no issue of Printf being interrupted on your debug screen.
in this foreground loop we process each state machine sequentially, much like a Multitasking solution.
the down side is we never sleep, but in our case we have power to burn.
Our unit draws 6 Watts since we have real work to do, the processor only draws 60mA at 3.3V is 0.2Watts
Sleeping will drop that to about 1/3 (I guess), so we save 0.13Watts if we sleep.
not worth the huge debug issues when switching tasks in the middle of a print statement.
2018-05-15 1:25 AM
another reason to never use multi tasking.
IMHO a bit too broad of a statement.
There do exist processors with multiple physical cores, which are only properly exploited with a multitasking OS.
But for a plain Cortex M, I agree.
And comprehending multiple, concurrent processes (including it's consequences on data handling) is quite a task ...