cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 timer question?

Dick Lin
Senior

Hi,

I am trying to use either TIM13 or TIM14 but the ISR never get trigger.

My questions are

  • Why the ISR routine never trigger? Is there anything else need be set?
  • how to control the timer? what's the prescaler, period mean?
  • If I want setup the timer trigger say every 10 ms how to?

Thx

****

startup_stm32f407xx.s

 .word   TIM8_UP_TIM13_IRQHandler     /* TIM8 Update and TIM13    */     

 .word   TIM8_TRG_COM_TIM14_IRQHandler   /* TIM8 Trigger and Commutation and TIM14 */

/* TIM13 init function */

void MX_TIM13_Init(void)

{

 htim13.Instance = TIM13;

 htim13.Init.Prescaler = 0;

 htim13.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim13.Init.Period = 0;

 htim13.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 if (HAL_TIM_Base_Init(&htim13) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

}

/* TIM14 init function */

void MX_TIM14_Init(void)

{

 htim14.Instance = TIM14;

 htim14.Init.Prescaler = 0;

 htim14.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim14.Init.Period = 0;

 htim14.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 if (HAL_TIM_Base_Init(&htim14) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

}

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8

Setting Prescaler and Period is going to result in the TIM not clocking...

The Prescaler and Period are divisors. You write a value as N-1, so zero means divide by ONE

TIMEBASE = (APBxTIMCLK / (Prescaler + 1)) / (Period + 1)

For 10 ms, you want 100 Hz

If the TIM is clocking at 84 MHz, that means 84,000,000 / 100 or 840,000 ticks to describe 10ms (0.01s)

Suggest a Prescaler of 840-1 (839) and Period of 1000-1 (999)

 /*##-2- Start the TIM Base generation in interrupt mode ####################*/

 if (HAL_TIM_Base_Start_IT(&TimHandle) != HAL_OK)

 {

   /* Starting Error */

   Error_Handler();

 }

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Dick Lin
Senior

Doesn't seems working, seems going nowhere in HAL_TIM_Base_Start_IT(). After I pause the execution, see below message.

Program received signal SIGINT, Interrupt.

0x08000fbe in main () at ..\Src\main.c:101

101  if (HAL_TIM_Base_Start_IT(&htim10) != HAL_OK)

My main() is pretty simple, just testing the TIM.

Any thoughts?

Thx

int main(void)

{

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* Configure the system clock */

 SystemClock_Config();

 MX_GPIO_Init();

 HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_0 | GPIO_PIN_8 | GPIO_PIN_9);

 /* Initialize all configured peripherals */

 MX_TIM10_Init();

 /*##-2- Start the TIM Base generation in interrupt mode ####################*/

 if (HAL_TIM_Base_Start_IT(&htim10) != HAL_OK)

 {

  /* Starting Error */

  Error_Handler();

 }

 while (1)

 {

 }

}

>>Any thoughts?

You've got interrupt handler code?

You've enabled the TIM clocks somewhere?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Dick Lin
Senior

I do have init code and ISR code. Anything else? Thx

/* TIM2 init function */

void MX_TIM2_Init(void)

{

 TIM_ClockConfigTypeDef sClockSourceConfig;

 TIM_MasterConfigTypeDef sMasterConfig;

 htim2.Instance = TIM2;

 htim2.Init.Prescaler = 840 - 1;

 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim2.Init.Period = 1000 - 1;

 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;

 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

}

/* TIM10 init function */

void MX_TIM10_Init(void)

{

 htim10.Instance = TIM10;

 htim10.Init.Prescaler = 840-1;

 htim10.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim10.Init.Period = 1000-1;

 htim10.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 if (HAL_TIM_Base_Init(&htim10) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

}

/* TIM11 init function */

void MX_TIM11_Init(void)

{

 htim11.Instance = TIM11;

 htim11.Init.Prescaler = 840-1;

 htim11.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim11.Init.Period = 1000-1;

 htim11.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 if (HAL_TIM_Base_Init(&htim11) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

}

void TIM1_UP_TIM10_IRQHandler()

{

uint32_t test = 0 ;

}

void TIM1_TRG_COM_TIM11_IRQHandler()

{

uint32_t test = 0 ;

}

void TIM2_IRQHandler()

{

uint32_t test = 0 ;

}

The IRQ Handlers would need to clear the sources otherwise they'll keep re-entering.

You configure the NVIC anywhere?

 /*##-2- Configure the NVIC for TIMx ########################################*/

 /* Set Interrupt Group Priority */

 HAL_NVIC_SetPriority(TIM2_IRQn, 4, 0);

 /* Enable the TIMx global Interrupt */

 HAL_NVIC_EnableIRQ(TIM2_IRQn);

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Dick Lin
Senior

Seems working now adding HAL_NVIC_EnableIRQ.

Does the HAL_TIM_IRQHandler clear the interrupt source?

void TIM1_UP_TIM10_IRQHandler()

{

HAL_TIM_IRQHandler(&htim10);

}

Yes, the mechanics there is that the HAL manages things, and then uses a call-back you supply depending on the source of the interrupt.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Dick Lin
Senior

Thank you so much. I have it working now. Thx