cancel
Showing results for 
Search instead for 
Did you mean: 

CAN BUS Code gets stuck at Activate the corresponding transmission request

Kaveh
Associate III

Hello,

My code gets stuck in "Activate the corresponding transmission request" when calling "HAL_FDCAN_AddMessageToTxFifoQ"

Here is where it actually gets stuck in stm32h7xx_hal_fdcan.c:

/* Activate the corresponding transmission request */
      hfdcan->Instance->TXBAR = ((uint32_t)1 << PutIndex);

CAN Init:

void CAN1_Init(void)
{
	CAN1.Instance = FDCAN1;
	CAN1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
	CAN1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK;		// EXTERNAL Means FDCAN treats its own transmitted messages as received
															// messages
 
	CAN1.Init.AutoRetransmission = ENABLE;
	CAN1.Init.NominalPrescaler = 3;		// Setting values for 500k bps
	CAN1.Init.NominalSyncJumpWidth = 1;
	CAN1.Init.NominalTimeSeg1 = 2;
	CAN1.Init.NominalTimeSeg2 = 2;
	CAN1.Init.TxBuffersNbr = 64;
	CAN1.Init.TxEventsNbr = 32;
	CAN1.Init.TxFifoQueueElmtsNbr = 32;
	CAN1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
	CAN1.Init.TxElmtSize = FDCAN_DATA_BYTES_16;
	CAN1.Init.MessageRAMOffset = 0;
	CAN1.Init.RxBuffersNbr = 64;
	CAN1.Init.RxFifo0ElmtsNbr = 64;
	CAN1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_16;
 
	if (HAL_FDCAN_Init(&CAN1) != HAL_OK)
	  {
	    Error_Handler();
	  }
 
}

CAN transmit:

void CAN1_TX(void)
{
	FDCAN_TxHeaderTypeDef TX_Header;
 
	uint8_t CAN_Msg_Ptr[5] = {'H', 'E', 'L', 'L', 'R'};
 
	TX_Header.DataLength = 1;
	TX_Header.Identifier = 0x7DF;
	TX_Header.IdType = FDCAN_STANDARD_ID;
	TX_Header.TxFrameType = FDCAN_DATA_FRAME;
	TX_Header.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
	TX_Header.BitRateSwitch = FDCAN_BRS_OFF;
	TX_Header.FDFormat = FDCAN_CLASSIC_CAN;
	TX_Header.TxEventFifoControl = FDCAN_STORE_TX_EVENTS;
	TX_Header.MessageMarker = 0x00;
 
	if (HAL_FDCAN_AddMessageToTxBuffer(&CAN1, &TX_Header, CAN_Msg_Ptr, FDCAN_TX_BUFFER0) != HAL_OK)
	  {
	    Error_Handler();
 
	  }
 
}

1 ACCEPTED SOLUTION

Accepted Solutions
Kaveh
Associate III

It was an endless loop. Oddly enough I made bellow changes in the CAN init and issue is fixed.

Basically changing the Nominal to Data in all bellow line.

	CAN1.Init.DataPrescaler = 3;		// Setting values for 500k bps
	CAN1.Init.DataSyncJumpWidth = 1;
	CAN1.Init.DataTimeSeg1 = 2;
	CAN1.Init.DataTimeSeg2 = 2;

View solution in original post

2 REPLIES 2
Ozone
Lead III

"gets stuck" is not quite an exact description.

Does it end up in a fault handler, or in an endless loop ?

Try switching to instruction step / assembler view in your debugger, and single-step through the associated instructions.

Kaveh
Associate III

It was an endless loop. Oddly enough I made bellow changes in the CAN init and issue is fixed.

Basically changing the Nominal to Data in all bellow line.

	CAN1.Init.DataPrescaler = 3;		// Setting values for 500k bps
	CAN1.Init.DataSyncJumpWidth = 1;
	CAN1.Init.DataTimeSeg1 = 2;
	CAN1.Init.DataTimeSeg2 = 2;