cancel
Showing results for 
Search instead for 
Did you mean: 

BUG in RM0394 Rev 4, regarding timer (TIM2) synchronization.

michal.matejasko
Associate II

When trying to synchronize (cascade) timers, specifically wanting TIM1 to provide clock for the TIM2, there is a bug in the reference manual RM0394 Rev 4.

The bug is in the recipe in the section 27.3.19, page 857, called Using one timer as prescaler for another timer, point 2.:

"2. To connect the TRGO output of TIMy to TIMz, TIMz must be configured in slave mode

using ITR2 as internal trigger. You select this through the TS bits in the TIMz_SMCR

register (writing TS=010)."

Instead of using internal trigger 2 (ITR2) as stated above, the user should use internal trigger 0 (ITR0), as stated in the Table 136 on the page 867. Moreover, there is no Internal Trigger 2 option for the TIM2/TIM3.

Sincerely,

Michal Matejasko

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello @michal.matejasko​ ,

I will take a look on your report issue and come back to you soon.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen