.bin file generated by GCC too large
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-08 4:34 AM
Hi ST community members
We are working on the optimization of a project's code running on STM32F429ZIT6 �C, in terms of speeding execution, or minimizing latencies due to memory access competition.
Our solution is to reorganize the code by assigning each AHB-bus-matrix's used master to the appropriate SRAM memory block.
To do that, our linker file is reorganized also, and buffers in our code are replaced in the appropriate sections.
But surprisingly, the .bin file generated is 384MB sized.
The gcc --version output is : (Sourcery CodeBench Lite 2014.05-28) 4.8.3 20140320 (prerelease)
Changes done are as follows:
* ucHeap[ TOTAL_HEAP_SIZE ] __attribute__((section('.bss_SRAM1'))); // FreeRTOS heap (
heap
4) placed in SRAM1.* Our Ethernet driver's DMA descriptors, TX and RX buffers placed in SRAM2.
* Other miscellaneous critical buffers placed in CCM RAM.
* remaining data (.data and .bss) placed in SRAM3.
You can see attached the sections.ld, mem.ld and a simplified makefile (without projects includes and sources) in the ldscripts.rar.
The data sections sizes generated by the compilation process are as follows:
section size addr
.isr_vector 824 134217728._inits 4 134218552.flashtext 0 134218556.text 273296 134218560.ARM.exidx8 134491856.data 1916 0.data_CCMRAM 36 268435456.bss_CCMRAM 7560 268435496.bss_SRAM1 10240 536870912.bss_SRAM2 12544 536985600.bss 49552 1920.noinit 0 51472._check_stack 256 51472.comment 70 0.ARM.attributes 53 0.debug_aranges 15592 0.debug_info 528968 0.debug_abbrev 56895 0.debug_line 234916 0.debug_frame 55916 0.debug_str 629362 0.debug_ranges 14184 0.debug_macro 186126 0Total 2078318
Thanks for help.
#stm32f429 #gcc-linker- Labels:
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-08 5:20 AM
The gcc --version output is : (Sourcery CodeBench Lite 2014.05-28) 4.8.3 20140320 (prerelease)
Not quite a recent version, but might work.
But surprisingly, the .bin file generated is 384MB sized.
As a first step, I would check the map file, and identify the causal source of your problem.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-08 7:34 AM
CCM and SRAM are 256MB apart, .BIN files are NOT sparse and will thus describe all the memory between and including the two regions. If you want a sparse file, use a .HEX or .DFU
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
‎2017-05-08 9:54 AM
Fully agree with Clive, BIN is a contiguous block of data without any start address: Avoid it like pest !
Motorola S19 or Intel HEX text format will have only relevant bits of memories stored with their address location.
Tip: The HEX/S19 file can be used in STV Link Utility to have in a single file both the internal and external serial flash memory for example for some discovery boards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-08 12:35 PM
Custom bootloaders like Arduino or mbed usually work with BIN files.
Full knowledge of the target's address space has then to be present in the loader.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-08 12:56 PM
Too bad it was not designed with futureproofing in mind.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-11 2:22 AM
Hi guys, thanks for your help. And sorry for last response
I generated the .hex output using the command
#@echo 'Creating Hex file : $@' @$(OBJCOPY) -O ihex $(EXE_DIR)/$(BINARYNAME).out $(EXE_DIR)/$(BINARYNAME).hexThe hex file doesn't work either when downloaded into the µC Flash, no execution, and debug doesn't work on our PC with ST-LINK/V2 (under eclipse) even after several trials and forum search ....Actually we used a trick to overcome the issue, we've declared the '
ucHeap' and the '
Ethernet driver's DMA descriptors, TX and RX buffers' as they were ST Hardware registers, we used the same manner CMSIS declared the chip hardware registers.
Example for the RTC's SSR register:#define PERIPH_BASE ((uint32_t)0x40000000) /*!< Peripheral base address in the alias region */
#define APB1PERIPH_BASE PERIPH_BASE
#define RTC_BASE (APB1PERIPH_BASE + 0x2800)
#define RTC ((RTC_TypeDef *) RTC_BASE)
typedef struct
{ __IO uint32_t WPR; /*!< RTC write protection register, Address offset: 0x24 */ __IO uint32_t SSR; /*!< RTC sub second register, Address offset: 0x28 */ __IO uint32_t SHIFTR; /*!< RTC shift control register, Address offset: 0x2C */} RTC_TypeDef;xDevice[u8DvInd].u8DataRxSeq = (uint8)((RTC->SSR)&0xFF);
the linker file didn't change, just the amount of RAM were decreased to fit only SRAM3.
This comes unfortunately by sacrificing about 8k of RAM precious in future project expand or developments.Does anyone have an idea to elegantly use the GCC linker file without the huge .bin generated ? we can as a consequence optimize the RAM used.
Thanks.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-11 4:57 AM
You don't have a SRAM3 memory region defined in mem.ld, so the linker fell back to default and assigned it to address 0, as witnessed by
section size addr .data 1916 0
.bss 49552 1920.noinit 0 51472._check_stack 256 51472As the SRAM3 is not physically at that address, it can't work.
Furthermore, the compiler tags variables with explicitly assigned section as executable (don't ask me why), thus objcopy copies them out into hex/bin, unless explicitly told not to using the -R switch.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-11 5:13 AM
@$(OBJCOPY) -O ihex $(EXE_DIR)/$(BINARYNAME).out $(EXE_DIR)/$(BINARYNAME).hex
The hex file doesn't work either ...No wonder, this is a self-defeating approach.
Your bin file contains way too much data, for addresses not specified for the target. Converting that .bin file to a .hex file is not addressing the issue.
How did you create this bin file in the first place ?
I suggest to create the native format (probably ELF), and convert this to .Hex or .s19, instead of .bin. The objcopy command would do as well.
.. when downloaded into the µC Flash, no execution, and debug doesn't work on our PC with ST-LINK/V2 (under eclipse) even after several trials and forum search ....
I think we better try to address issues one at a time, the failure to debug can well be caused by your oversized .bin file.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-29 3:09 AM
I had similar issue with the STM32F746G Discovery demo code for LwIP. I founf an error in the linker map supplied by ST which forgot to put a NOLOAD attribute for the ethernet buffers so the linker was placing data into the SRAM locations as well as FLASH so making the binary 393MB.
If you have a linker script check for areas mapped to the SRAM and see if this may also the the case.