cancel
Showing results for 
Search instead for 
Did you mean: 

Baud rate of 4Mbps

000harsha
Associate II

Hello everybody,

This is my first post hope i wll get the answer.

I am building a spectrometer for which i am using a stm32f401re board and i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps so do i need to use 4Mbps baud rate to read that and if so how to achieve such higher baud rates.

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions

From ds:

AScha3_0-1720601963254.png

 

 

So whats the problem?

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
SofLit
ST Employee

Hello and welcome to the community.


i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps

Not clear! Is it over a protocol communication? which one?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Yes it is over UART

From ds:

AScha3_0-1720601963254.png

 

 

So whats the problem?

If you feel a post has answered your question, please click "Accept as Solution".