cancel
Showing results for 
Search instead for 
Did you mean: 

Baud rate of 4Mbps

000harsha
Associate II

Hello everybody,

This is my first post hope i wll get the answer.

I am building a spectrometer for which i am using a stm32f401re board and i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps so do i need to use 4Mbps baud rate to read that and if so how to achieve such higher baud rates.

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions

From ds:

AScha3_0-1720601963254.png

 

 

So whats the problem?

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
SofLit
ST Employee

Hello and welcome to the community.


i need to sample the data coming from a sensor at 250kHz which nearly gives a data rate of nearly 4Mbps

Not clear! Is it over a protocol communication? which one?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Yes it is over UART

From ds:

AScha3_0-1720601963254.png

 

 

So whats the problem?

If you feel a post has answered your question, please click "Accept as Solution".