Basic UART Interrupt TX causes system crash STM32F767
Hey All,
I'm a bit at my wits end here trying to debug a pesky issue I'm having with a very basic interrupt mode UART transmit. The issue is that when I call HAL_UART_Transmit_IT(), it causes the whole chip to lock up. I've spent literally the entire day running through example code from the STM32CubeMX, looking at tutorials online, stepping through annotated assembly code line by line, reading ST application notes, and haven't yet found the root cause. If someone wouldn't mind taking a quick look at what I have it'd be much appreciated. I could really use a fresh set of eyes.
I'm running on a NUCLEO-F767ZI board with the latest ST-Link debugger/programmer firmware.
/* Just assume these GPIO objects work as intended. They have been well vetted in other projects of mine. */
GPIOClass testPin(GPIOA, PIN_15, HIGH_SPD, NO_ALTERNATE);
GPIOClass txPin(GPIOE, PIN_8, ULTRA_SPD, GPIO_AF8_UART7);
GPIOClass rxPin(GPIOE, PIN_7, ULTRA_SPD, GPIO_AF8_UART7);UART_HandleTypeDef huart7;
char message[] = 'Hello World';
uint8_t data = 0x33;int main(void){ HAL_Init(); testPin.mode(OUTPUT_PP); /*GPIO Config */ txPin.mode(ALT_PP, PULLUP); rxPin.mode(ALT_PP, PULLUP); /*Interrupt Config */ HAL_NVIC_DisableIRQ(UART7_IRQn); HAL_NVIC_ClearPendingIRQ(UART7_IRQn); HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_0); HAL_NVIC_SetPriority(UART7_IRQn, 0, 0); HAL_NVIC_EnableIRQ(UART7_IRQn); /*UART Config */ __UART7_CLK_ENABLE(); huart7.Instance = UART7; huart7.Init.BaudRate = 115200; huart7.Init.WordLength = UART_WORDLENGTH_8B; huart7.Init.StopBits = UART_STOPBITS_1; huart7.Init.Parity = UART_PARITY_NONE; huart7.Init.Mode = UART_MODE_TX_RX; huart7.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart7.Init.OverSampling = UART_OVERSAMPLING_16; huart7.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart7.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart7) != HAL_OK) ASSERT_ERROR_BKPT; // asm('bkpt 255') /* Calling the interrupt version crashes the whole chip */ //HAL_UART_Transmit_IT(&huart7, &data, 1); for (;;) {/* Calling the blocking version works just fine */
HAL_UART_Transmit(&huart7, (uint8_t *)message, strlen(message), HAL_MAX_DELAY); testPin.toggle(); HAL_Delay(10); }}void UART7_IRQHandler(void)
{ HAL_UART_IRQHandler(&huart7);}#stm32f7 #crash #interrupt-issue