Skip to main content
ykn
Associate III
April 6, 2023
Question

bank swapping in stm32h745

  • April 6, 2023
  • 3 replies
  • 2000 views

Hi,

I want to use OTA in stm32h743, for that I need to switch between two bank after flash write, as per reference manual

//HAL_FLASH_OB_Lock();
	HAL_FLASH_OB_Unlock();
 
	/* Set OPTSTRT Bit */
	SET_BIT(FLASH->OPTSR_PRG, FLASH_OPTCR_SWAP_BANK);
	/* Wait for OB change operation to be completed */
	status = FLASH_OB_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE);
 
 
	/* Set OPTSTRT Bit */
	SET_BIT(FLASH->OPTCR, FLASH_OPTCR_OPTSTART);
	/* Wait for OB change operation to be completed */
	status = FLASH_OB_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE);
	if(READ_BIT(FLASH->OPTSR_CUR, FLASH_OPTCR_SWAP_BANK) != 0U)
		{
			UARTSendString(RS232_PORT, (unsigned char*)"Bit Set \r\n\r\n");
		}
	//__disable_irq();
	HAL_NVIC_SystemReset();

i wrote some code

HAL_StatusTypeDef HAL_FLASH_OB_Unlock(void)
{
 if(READ_BIT(FLASH->OPTCR, FLASH_OPTCR_OPTLOCK) != 0U)
 {
 /* Authorizes the Option Byte registers programming */
 WRITE_REG(FLASH->OPTKEYR, FLASH_OPT_KEY1);
 WRITE_REG(FLASH->OPTKEYR, FLASH_OPT_KEY2);
 
 /* Verify that the Option Bytes are unlocked */
 if (READ_BIT(FLASH->OPTCR, FLASH_OPTCR_OPTLOCK) != 0U)
 {
 return HAL_ERROR;
 }
 }
 
 return HAL_OK;
}

but it is not working please guide me for this

This topic has been closed for replies.

3 replies

ST Technical Moderator
April 6, 2023

Hello @ykn​ ,

I recommend you this article that will help you on how to configure swap bank based on an STM32H7 example:

Hope this helped you.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ykn
yknAuthor
Associate III
April 6, 2023

I have almost done the above thing, Now I got the error

Break at address "0x812bb84" with no debug information available, or outside of program code.

currently working on bank 1 and want switch to bank 2. One addition thing i have added is

HAL_NVIC_SystemReset();

this functin , the manual implied that you need to reset the sysytem.

Thankinh you

ykn
yknAuthor
Associate III
April 7, 2023

I came to know that, the break point address is hardfault

void HardFault_Handler(void)
{
 8100a26:	b480 	push	{r7}
 8100a28:	af00 	add	r7, sp, #0
 /* USER CODE BEGIN HardFault_IRQn 0 */
 
 /* USER CODE END HardFault_IRQn 0 */
 while (1)
 8100a2a:	e7fe 	b.n	8100a2a <HardFault_Handler+0x4>

why should I get hardfault.

Checklist

  1. linker script change
MEMORY
{
 FLASH (rx) : ORIGIN = 0x08100000, LENGTH = 1024K
 DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
 RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
 RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
 RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
 ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}
  • Vector tab address changed
#if defined(USER_VECT_TAB_ADDRESS)
#if defined(DUAL_CORE) && defined(CORE_CM4)
/*!< Uncomment the following line if you need to relocate your vector Table
 in D2 AXI SRAM else user remap will be done in FLASH BANK2. */
/* #define VECT_TAB_SRAM */
/*#if defined(VECT_TAB_SRAM)*/
#define VECT_TAB_BASE_ADDRESS D2_AXISRAM_BASE /*!< Vector Table base address field.
 This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
 This value must be a multiple of 0x200. */
#else
#define VECT_TAB_BASE_ADDRESS FLASH_BANK2_BASE /*!< Vector Table base address field.
 This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00100000U /*!< Vector Table base offset field.
 This value must be a multiple of 0x200. */
#endif /* VECT_TAB_SRAM */
#else
/*!< Uncomment the following line if you need to relocate your vector Table
 in D1 AXI SRAM else user remap will be done in FLASH BANK1. */
/* #define VECT_TAB_SRAM */
#if defined(VECT_TAB_SRAM)
#define VECT_TAB_BASE_ADDRESS D1_AXISRAM_BASE /*!< Vector Table base address field.
 This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
 This value must be a multiple of 0x200. */
#else
#define VECT_TAB_BASE_ADDRESS FLASH_BANK1_BASE /*!< Vector Table base address field.
 This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
 This value must be a multiple of 0x200. */
#endif /* VECT_TAB_SRAM */
#endif /* DUAL_CORE && CORE_CM4 */
  • land last
#define FLASH_BANK1_BASE (0x08000000UL) /*!< Base address of : (up to 1 MB) Flash Bank1 accessible over AXI */
#define FLASH_BANK2_BASE (0x08100000UL) /*!< Base address of : (up to 1 MB) Flash Bank2 accessible over AXI */
#define FLASH_END (0x081FFFFFUL) /*!< FLASH end address */
 
/* Legacy define */
#define FLASH_BASE FLASH_BANK2_BASE

Please some one guide where i am wrong.

I have done the same task using custom bootloader and that worked fine. buth same the thing i tried with bank swapping i got hardfault error.:expressionless_face: