2023-08-08 12:54 AM
Hi,
someone knows where the Backup SRAM is located on STM32H563 (at which address)? I didn't find it in the documentation.
Thanks
Solved! Go to Solution.
2023-08-08 1:59 AM - edited 2023-08-08 2:06 AM
Hello @Ez ,
Backup SRAM starts at address 0x4003_6400 to 0x4003_73FF (Non-Secure)
or
0x5003_6400 to 0x5003_73FF (Secure)
I will ask to add it inside the Reference Manual.
Best Regards,
Gwénolé
2023-08-08 1:59 AM - edited 2023-08-08 2:06 AM
Hello @Ez ,
Backup SRAM starts at address 0x4003_6400 to 0x4003_73FF (Non-Secure)
or
0x5003_6400 to 0x5003_73FF (Secure)
I will ask to add it inside the Reference Manual.
Best Regards,
Gwénolé
2023-08-08 11:40 PM
Thank you very much
2023-11-29 10:42 AM
i have same question about STM32F7 !
the Backup SRAM address is not listed in the RM0410 Rev 4
2023-11-29 11:19 AM
see ds , p. 104
2023-11-29 11:38 AM
correct, i found after i posted :face_with_tears_of_joy:
just difficult to find since not listed as 'backup SRAM' (instead of BKPSRAM)