cancel
Showing results for 
Search instead for 
Did you mean: 

Backup SRAM on STM32H563

Ez
Associate II

Hi,

someone knows where the Backup SRAM is located on STM32H563 (at which address)? I didn't find it in the documentation.

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
GwenoleB
ST Employee

Hello @Ez ,

Backup SRAM starts at address 0x4003_6400 to 0x4003_73FF (Non-Secure)
or 
0x5003_6400 to 0x5003_73FF (Secure)

I will ask to add it inside the Reference Manual.

Best Regards,
Gwénolé

View solution in original post

5 REPLIES 5
GwenoleB
ST Employee

Hello @Ez ,

Backup SRAM starts at address 0x4003_6400 to 0x4003_73FF (Non-Secure)
or 
0x5003_6400 to 0x5003_73FF (Secure)

I will ask to add it inside the Reference Manual.

Best Regards,
Gwénolé

Thank you very much

jerry_sandc
Associate III

i have same question about STM32F7 !

the Backup SRAM address is not listed in the RM0410 Rev 4

see ds , p. 104

AScha3_0-1701285510929.png

 

If you feel a post has answered your question, please click "Accept as Solution".

correct, i found after i posted  :face_with_tears_of_joy:

just difficult to find since not listed as 'backup SRAM' (instead of BKPSRAM)