2022-10-17 2:42 PM
Hi,
In my design, STM32F7 MCU communicates with FPGA via FSMC bus. FPGA emulates an asynchronous NOR flash. It was noticed that when MCU does back-to-back writes (2 lines of assembly code for each write) to the same FSMC address only the last 16-bit word appears on the FSMC bus. It seems that the first few writes are optimized away. I did check the assembly code and it looks correct. Can you advise on this?
Regards
Gordon
2022-10-17 3:11 PM
Perhaps write buffers, or caching?
Perhaps change the MPU configuration for the address space the FPGA lives in, so all writes reflect, and it's not treated as a memory device.