2018-03-23 1:15 AM
For mipi DSI validation using the B-LCD40-DSI1 daughterboard.
We need the driver code and mipi panel controller register configuration for this mipi panel.
2018-03-23 1:21 AM
You realise that this is essentially a user-to-user forum?
If you want direct, priority support then you need to contact your ST or Distributor FAE
Please respond us as soon as possible
http://www.catb.org/~esr/faqs/smart-questions.html#urgent
We are validating the (sic) SoC in FPGA platform
What SoC ?
What 'FPGA platform' ?
we need LCD controller datasheet
So contact the LCD controller manufacturer?
EDIT
This:
?2018-03-23 5:24 AM
STM32Cube_FW_F7_V1.9.0\Drivers\BSP\STM32F769I-Discovery\stm32f769i_discovery_lcd.c
STM32Cube_FW_F7_V1.9.0\Drivers\BSP\Components\otm8009a\otm8009a.c
2018-03-26 2:04 AM
Hi Clive One,
Thanks for your reply.
we are not using any STM Evaluation boards, we are using the only MIPI-DSI LCD Panel.For this MIPI DSI LCD Panel do we need driver ?
what ever you suggested c files
stm32f769i_discovery_lcd.c
This c file contains bridge chip (
ADV7533)
configuration and DSI to HDM adapter code.
But we are using the another DSI Controller , we implemented the driver for
DSI Controller but Panel we did not configured ant thing. Really is required driver for Panel.
Thanks
Viswa
2018-03-26 5:23 AM
viswanath reddy wrote:
we are not using any STM Evaluation boards
Are you suing any STM32 at all?
Really is required driver for Panel.
What is provided by ST is in the files
Turvey.Clive.002
mentioned.If youcan't work from there, then you're going to have to contact the panel manufacturer for support ...
2018-03-26 6:59 AM
The information contained in the C files is relatively portable in its application.
Pretty sure the panel specific stuff is configured in the OTM8009A file, seeing as it is the controller attached to the display.
http://orientdisplay.com/pdf/OTM8009A.pdf