Skip to main content
Nitin
Associate III
Jan 12, 2024 1:10 PM UTC
Solved

Azure RTOS Integration in B-U585-IOT2A Bootloader Environment

Hello ST, I am trying to integrate ThreadX into TFM_Appli-NonSecure project. Mostly I am able to integrate it and execute but to make a thread run, I have to comment _tx_initialize_low_level(); API in _tx_initialize_kernel_enter() function.

This all work smoothly until I try thread context switching. My initial understanding assumption says pendsv_hander is not getting called.

Could I get some more insight to resolve this issue as there is no direct example available for this.

This topic has been closed for replies.
Guillaume K
Guillaume KBest answer
ST Employee
Jan 12, 2024 4:35 PM UTC

Hello

Did you look at X-CUBE-AZURE - Microsoft Azure software expansion for STM32Cube - STMicroelectronics ?

It has an example of TFM NS application with ThreadX.

it's in Projects\B-U585I-IOT02A\Applications\TFM_Azure_IoT

normally you shouldn't comment _tx_initialize_low_level().

ThreadX requires to use the SysTick interrupt for its own tick (10 ms). it is done in _tx_initialize_low_level.

There is conflict with STM32 HAL that uses Systick for its own tick (1 ms).

Solution is to use additional timer TIM6 instead of SysTick for HAL tick.

See examples with ThreadX (especially Netxduo examples) in STM32 Cube U5.

Also because it is a TrustZone non-secure app there are some ThreadX sources and #define that must be added in the project.

tx_thread_secure_stack_allocate/_free.c, txe_thread_secure_stack_allocate/_free.c

tx_thread_secure_stack_initialise/_build.s

add define TX_SINGLE_MODE_NON_SECURE=1 at project level for C compiler

add define TX_SINGLE_MODE_NON_SECURE for assembler files

see Chapter 2 - Installing ThreadX support for ARMv8-M | Microsoft Learn

 

 

17 replies

Visitor II
Jan 12, 2024 1:29 PM UTC

Since you suspect that the PendSV handler is not getting called, verify the configuration related to PendSV in your setup. Make sure that the vector table is correctly set up to point to the correct PendSV handler function.

Nitin
NitinAuthor
Associate III
Jan 12, 2024 3:07 PM UTC

Thanks for replying, everything seems correct to me. One of the main reason behind this can be some TF-M violation.

Nitin
NitinAuthor
Associate III
Jan 12, 2024 2:18 PM UTC

To be precise, after this call MCU is getting reset in loop

/* Set PendSV to invoke ThreadX scheduler. */

*((volatile ULONG *) 0xE000ED04) = ((ULONG) 0x10000000);

Guillaume K
Guillaume KBest answer
ST Employee
Jan 12, 2024 4:35 PM UTC

Hello

Did you look at X-CUBE-AZURE - Microsoft Azure software expansion for STM32Cube - STMicroelectronics ?

It has an example of TFM NS application with ThreadX.

it's in Projects\B-U585I-IOT02A\Applications\TFM_Azure_IoT

normally you shouldn't comment _tx_initialize_low_level().

ThreadX requires to use the SysTick interrupt for its own tick (10 ms). it is done in _tx_initialize_low_level.

There is conflict with STM32 HAL that uses Systick for its own tick (1 ms).

Solution is to use additional timer TIM6 instead of SysTick for HAL tick.

See examples with ThreadX (especially Netxduo examples) in STM32 Cube U5.

Also because it is a TrustZone non-secure app there are some ThreadX sources and #define that must be added in the project.

tx_thread_secure_stack_allocate/_free.c, txe_thread_secure_stack_allocate/_free.c

tx_thread_secure_stack_initialise/_build.s

add define TX_SINGLE_MODE_NON_SECURE=1 at project level for C compiler

add define TX_SINGLE_MODE_NON_SECURE for assembler files

see Chapter 2 - Installing ThreadX support for ARMv8-M | Microsoft Learn

 

 

Nitin
NitinAuthor
Associate III
Jan 18, 2024 7:03 AM UTC

Thanks Guillaume for the detailed reply.

Things are much clear now. But I still have some problem to be resolved(may be last one). Actually I have some issue with below statement from the link provided.

"The file tx_thread_secure_stack.c must be added to the secure application."

It's not clear to me actually and I am getting undefined reference for all the functions defined in this file.

(.text+0x60): undefined reference to `_tx_thread_secure_stack_context_save'
(.text+0x90): undefined reference to `_tx_thread_secure_stack_context_restore'
(.text+0xfe): undefined reference to `_tx_thread_secure_mode_stack_allocate'
(.text+0x110): undefined reference to `_tx_thread_secure_mode_stack_free'
(.text+0x120): undefined reference to `_tx_thread_secure_mode_stack_initialize'

Moreover Projects\B-U585I-IOT02A\Applications\TFM_Azure_IoT is not directly compiling. So not able to take much help from it.

Guillaume K
ST Employee
Jan 18, 2024 8:36 AM UTC

Hello Nitin

regarding the missing functions you mention (_tx_thread_secure_stack_context_save, etc), did you define TX_SINGLE_MODE_NON_SECURE for C compiler AND also for the assembler ?

what IDE/compiler are you using ?

In fact, some of the tx_thread_secure_* files are not really used in case of non-secure application. I guess Microsoft suggest to put everything in the project in case you switch it to secure side.

 

- What do you mean by "Projects\B-U585I-IOT02A\Applications\TFM_Azure_IoT is not directly compiling. " ?

In this package, several other projects must be compiled before the non secure application (bootloader, TFM secure application, etc).

If you use IAR EWARM , you must run the batch build (F8) that will compile the project in correct order.

If you use STM32CubeIDE, in TFM_Appli project normally there are references to other projects that will make them compile before. You have to import in your workspace all the STM32CubeIDE projects under Projects\B-U585I-IOT02A\Applications\TFM_Azure_IoT .

If you are using STM32CubeIDE version 1.14.0 , try to switch to 1.14.1 released recently. Version 1.14.1 corrects problems when running shell commands from STM32CubeIDE. 

 

Jocelyn RICARD
ST Employee
Jan 12, 2024 5:23 PM UTC

Hello Nitin,

on top of Guillaume's feedback, one other point to check is relative to interrupt vector pointer.

In _tx_initialize_low_level you reference g_pfnVectors (at lines 527 and 538)

 /* Setup Vector Table Offset Register. */
 MOV r0, #0xE000E000 // Build address of NVIC registers
 LDR r1, =g_pfnVectors // Pickup address of vector table
 STR r1, [r0, #0xD08] // Set vector table address

 /* Enable the cycle count register. */
 LDR r0, =0xE0001000 // Build address of DWT register
 LDR r1, [r0] // Pickup the current value
 ORR r1, r1, #1 // Set the CYCCNTENA bit
 STR r1, [r0] // Enable the cycle count register

 /* Set system stack pointer from vector value. */
 LDR r0, =_tx_thread_system_stack_ptr // Build address of system stack pointer
 LDR r1, =g_pfnVectors // Pickup address of vector table
 LDR r1, [r1] // Pickup reset stack pointer
 STR r1, [r0] // Save system stack pointer

 

But in actual interrupt vectors definition in startup_stm32u5xx.c of non secure application example, you have 

extern const pFunc __VECTOR_TABLE[];
 const pFunc __VECTOR_TABLE[] __VECTOR_TABLE_ATTRIBUTE = {
 (pFunc)(&__INITIAL_SP), /* Initial Stack Pointer */
 Reset_Handler, /* Reset Handler */
 NMI_Handler, /* -14: NMI Handler */

So you probably need to align the naming.

I didn't have time to double check but worth trying because your issue seems related to this

Best regards

Jocelyn

Nitin
NitinAuthor
Associate III
Jan 18, 2024 7:06 AM UTC

Thanks Jocelyn, you got it correctly. g_pfnVectors was one of the issue and it got resolved after replacing with __Vectors.

TDJ
Senior III
Jan 12, 2024 8:30 PM UTC

@Nitin Why do not you use the original Arm TF-M solution?
The reason I ask is because I just spend entire week testing TFM and SBSFU apps, going thorough all the docs to make sense out of it and then I learned that TFM has been recently removed from GitHub and, I assume, will not be supported anymore. Probably the same is true for SBSFU. See issue #37 & issue #38.

TF-M solution 2.0 is a state-of-the-art solution, contains preconfigured profiles for the following ST MPUs/boards:
b_u585i_iot02a
nucleo_l552ze_q
stm32h573i_dk
stm32l562e_dk
It is actively maintained (new commits everyday), is highly configurable, has own community supporting it, current roadmap and well documented releases  - which is not to be said about ST TFM app, probably based on relatively old TF-M 1.3. There is just one thing, as I found out, to understand how TF-M is supposed to be used one needs to study MCUboot design and PSA Certified Firmware Update API documents first (TF-M is really MCUBoot extension).

In my view, it is actually good that ST stopped supporting TFM because it clearly had no commitment, capacity and motivation to do it well enough. This effort could be much better spend on supporting the original Arm TF-M and own HAL. Maturity-wise ST is still where Microsoft used to be during Steve Ballmer era, still dreaming of total market domination, trying to provide own software everywhere (e.g. own Internet Explorer renderer) instead of focusing on HAL quality while contributing and collaborating anywhere else, where it would make much more sense.
I would happily pay 50% more for ST MCUs and would not even look at alternatives if they came with high quality HAL and examples, but currently this is not an option.

Just my 3 cents.

Pavel A.
Jan 14, 2024 9:33 PM UTC

@TDJ ST does support trustedfirmware.org, they are even listed as a Platinum member.  https://www.trustedfirmware.org/join/

 

 

TDJ
Senior III
Jan 15, 2024 7:39 AM UTC

@Pavel A. Correct, there is hope, on the list of TF-M maintainers there is one ST employee.

Nitin
NitinAuthor
Associate III
Jan 18, 2024 6:00 PM UTC

Hi Guillaume, I was doing one silly mistake. Actually I didn't included TX_SINGLE_MODE_NON_SECURE for the assembler.

 

Now,

  1. _tx_initialize_low_level() is not commented.

Nitin_5-1705598809586.png

 

  1. using additional timer TIM6 instead of SysTick for HAL tick.

Nitin_6-1705598809595.png

 

Nitin_7-1705598809598.png

 

 

  1. TX_SINGLE_MODE_NON_SECURE=1 is included in C compiler and assembler.

Nitin_8-1705598809600.png

 

Nitin_10-1705601702100.png

 

 

tx_thread_secure_stack_allocate/_free.c, txe_thread_secure_stack_allocate/_free.c, tx_thread_secure_stack_initialise/_build.s included(as I am able to compile my code.

 

I followed all these steps but still my application is not moving past

*((volatile ULONG *) 0xE000ED04) = ((ULONG) 0x10000000);

And device is resetting continously. Is there anything I am still missing!!!

 

Only doubt I have is, “The file tx_thread_secure_stack.c must be added to the secure application.” I have not added this file into secure area.

Nitin
NitinAuthor
Associate III
Jan 19, 2024 5:52 PM UTC

Hello ST, please guide me to resolve this issue. Is PendSV priority has to be changed to trigger the interrupt?

Guillaume K
ST Employee
Jan 22, 2024 8:20 AM UTC

Not sure why it doesn't work. I don't have your full project. It could be anything.

Did you compare with what is done in X-Cube-Azure package ?

Don't touch PendSV priority. it should be 15 (lowest).

TIM6 should be higher priority than PendSV (so for example 14).

 

Nitin
NitinAuthor
Associate III
Jan 22, 2024 3:35 PM UTC

Hi Guillaume, I have commented here in this thread. This thread is most relevant to my current blockage. If you could look into this.

I don't this their much work done on STM32U585 series, specially on TFM + BL setup. We are expecting active support from ST on this.

 

https://community.st.com/t5/stm32cubemx-mcus/stm32cubeide-1-7-mcu-package-l4-series-1-17-vtor-is-not/td-p/220563/page/2

Guillaume K
ST Employee
Jan 22, 2024 5:02 PM UTC

The thread you mention talks about customisation of interrupt vectors table address on STM32L4.

It is different on STM32U5 in TFM environment.

Do you have in your code the function SystemInit() in system_stm32u5xx.c? could you compare your code with reference TFM implementation in Projects/B-U585I-IOT02A/Applications/TFM/TFM_Appli/NonSecure/Core/Src/system_stm32u5xx.c, function SystemInit():

There should be only these lines:

void SystemInit(void)
{
/* FPU settings ------------------------------------------------------------*/
#if (__FPU_PRESENT == 1) && (__FPU_USED == 1)
SCB->CPACR |= ((3UL << 20U)|(3UL << 22U)); /* set CP10 and CP11 Full Access */
#endif
}

when comparing to "standard" system_stm32u5xx.c some code is removed.  the SCB->VTOR register is not modified directly in this file. also some clock settings are not changed. If the lines modifying SCB->VTOR are present then it could explain the problem.