cancel
Showing results for 
Search instead for 
Did you mean: 

Are there any examples that configure and use the Burst Mode Controller for HRTIM? I did not see any under the example selector.

CWatt.1
Associate
 
1 REPLY 1
Petr DAVID
ST Employee

Hello Cwatt.1,

I have found for you example that could be described as Multiphase demonstration overview. It is further described in HRTIM cookbook AN4539 page 42.

The demonstration starts in 5-phase mode. If the push-button is pressed, the demonstration mode changes so that all phase shedding options are scanned: from 5- to 1-phase, and finally burst mode. The example could be found in STM32F3Cube FW package under \Projects\ STM32F3348-Discovery\Examples\ HRTIM\HRTIM_Multiphase.

Please click on Select as Best if my reply fully answered your question. This will help other users with the same problem to find the solution faster!