2024-04-10 07:10 AM
Hi
In the reference manual, RM0481 rev1, for analog watchdog window it mentions SQRi and JSQRi registers. I can not find any descriptions about these registers.
Can someone help me clarifying this?
Br
Imre
Solved! Go to Solution.
2024-04-10 07:19 AM - edited 2024-04-10 07:21 AM
Hello @Imre
You can find details about those two registers on the section 26.4.11 "Channel selection (SQRx, JSQRx)" and pages from 1128 to 1134 of the RM0481
PS: use the last revision (Rev2).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-10 07:19 AM - edited 2024-04-10 07:21 AM
Hello @Imre
You can find details about those two registers on the section 26.4.11 "Channel selection (SQRx, JSQRx)" and pages from 1128 to 1134 of the RM0481
PS: use the last revision (Rev2).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-10 07:22 AM
Ah, ok I see it now 🙂 Thank you!
2024-04-10 07:24 AM - edited 2024-04-10 07:24 AM
Hello,
Starting from page 1128:
SQRi:
JSQR:
Meawhile, I think it woul be better to rename them with the corresponding naming used in the documentation starting by "ADC_"
For JSQR, there is only one regiter so no need to add "i" at the end.
I'm escalating this internally to confirm and get back to you with a feedback