2014-07-14 03:14 AM
Hi.
I need to get acquainted with AN4229, but can not find anything (except PDF file). please indicate where the files? Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-01-11 08:11 AM
The top level post is from 3 years ago
Might I suggest an approach like this for assigning staff and priorities to specific customers, projects and regions.
https://www.u-blox.com/en/project-information-form
2018-01-11 08:22 AM
Clive One wrote:
The top level post is from 3 years ago
Ha ha - so it is!
It was
Wolf.Colin
who just woke it up saying the ST in Germany were unresponsiveMaybe I would've noticed that if I wasn't restricted to this nasty 'Activity' view due to the current forum shambles ... ?
(or maybe not).
2018-01-11 08:23 AM
so I can't edit my post in this view!
2018-01-11 08:31 AM
Andrew, I agree. There are really a few exceptions where for some reasons we need to sign such a legal document. We should make it clear in the document.
2018-01-11 08:47 AM
Hello
vera.laurent
,can you tell something about the reason in this special case?
2018-01-11 08:58 AM
Typical reasons are the IP is covered by licensing or patent issues, or expresses stuff that is commercially sensitive or contains trade secrets (stuff you don't want disclosed in a patent, and can be used to invalidate others)
2018-01-11 09:05 AM
Yes, apparently 'Editing' is an advanced function, and the Action button offers no personal options, I could give you a badge if I wanted.
A lack of editing in all cases might be constructed as a violation of the ADA (Americans with Disabilities Act) as it doesn't provide reasonable accommodation for those with dyslexia or general clumsiness.
The 'Inbox' view generally seems to work for threads I'm participating in, and this provides age/chronology info.
2018-01-11 09:17 AM
Which one are you calling the 'inbox' view?
Why are there so many views? Seems like just an excuse for Jive justify taking ages to fix because it is, 'very complicated' ...
2018-01-11 09:36 AM
I click on the Bell, get the Inbox (full view selected, see form selected on upper right), then click on posts
2018-01-11 09:56 AM
OK - I see.
But from there (your 2nd screenshot), if I click the thread title, it gives an 'unexpected error' - although we have now come to expect that ...