cancel
Showing results for 
Search instead for 
Did you mean: 

AIS2DW12 and SMT32L0 high current

Zek_De
Senior

Hello everyone,

board consume too much energy when the acc wakeup and start to measure the tilt.

in Stop Mode : 5 uA

in Wake up : 280 uA

MCU setting for INT pin belong to acc : No pull up-down and rising-edge trigger

for CS pin push-pull and no pull up-down for MCU and for acc is pull up disconnection.

Is this current normal for operation according to code below

dev_ctx.write_reg = platform_write;
	dev_ctx.read_reg = platform_read;
	dev_ctx.handle = SPI1;
	delay_ms(k_BOOT_TIME);
	ais2dw12_device_id_get(&dev_ctx, &whoamI);
	if (whoamI != AIS2DW12_ID)
		while (1);
 
	/* Restore default configuration */
	ais2dw12_reset_set(&dev_ctx, PROPERTY_ENABLE);
 
	do
	{
		ais2dw12_reset_get(&dev_ctx, &rst);
	} while (rst);
 
	/* Start device configuration. */
	ais2dw12_i2c_interface_set(&dev_ctx, AIS2DW12_I2C_DISABLE);
	ais2dw12_spi_mode_set(&dev_ctx, AIS2DW12_SPI_4_WIRE);
	ais2dw12_cs_mode_set(&dev_ctx, AIS2DW12_PULL_UP_DISCONNECT);
//	ais2dw12_pin_polarity_set(&dev_ctx, AIS2DW12_ACTIVE_LOW);
//	ais2dw12_pin_mode_set(&dev_ctx, AIS2DW12_OPEN_DRAIN);
	ais2dw12_data_rate_set(&dev_ctx, AIS2DW12_XL_ODR_25Hz);
//	ais2dw12_data_ready_mode_set(&dev_ctx, AIS2DW12_DRDY_PULSED);
	ais2dw12_full_scale_set(&dev_ctx, AIS2DW12_2g);
//	ais2dw12_filter_path_set(&dev_ctx, AIS2DW12_LPF_ON_OUT);
//  ais2dw12_filter_bandwidth_set(&dev_ctx, AIS2DW12_ODR_DIV_4);
	ais2dw12_power_mode_set(&dev_ctx, AIS2DW12_PWR_MD_12bit);
	ais2dw12_wkup_dur_set(&dev_ctx, 1); // x * (1/ODR) = 40 ms
	ais2dw12_act_sleep_dur_set(&dev_ctx, 0); // 16*1/ODR = 640 ms 
	ais2dw12_wkup_threshold_set(&dev_ctx, 4); // 4*(FS/64) = 125 mg
//	ais2dw12_wkup_feed_data_set(&dev_ctx, AIS2DW12_HP_FEED);
	//set act-inact mode
	ais2dw12_act_mode_set(&dev_ctx, AIS2DW12_DETECT_ACT_INACT);
	ais2dw12_pin_int1_route_get(&dev_ctx, &int_route.ctrl4_int1);
  int_route.ctrl4_int1.int1_wu = PROPERTY_ENABLE;
  ais2dw12_pin_int1_route_set(&dev_ctx, &int_route.ctrl4_int1);

2 REPLIES 2
EARSL.1
Associate

hello, I have the same problem. Did you solve the problem?

Zek_De
Senior

Because of internal pull-up on communication line.