cancel
Showing results for 
Search instead for 
Did you mean: 

After activating the CMSIS Core and CMSIS DSP package in "Software packs" tab, I get the following errormessage:

JSchn.4
Associate III

Any help is highly appreciated!

2 REPLIES 2
JSchn.4
Associate III

"Logical Parser: syntax error detected in expression for ARM.CMSIS.5.5.0_M7 original expression:

(SliDTzliTZ$context&)

parser evaluation:

(0&

PKut.1
Associate

I can confirm the problem is present for CMSIS 5.8.0 and CubeMX 6.2.1.

LogicalParser: syntax error detected in expression for ARM.CMSIS.5.8.0 orignal expression: (SIiDtzIiTZ&) parser evaluation: (0&)

Also after installing CMSIS 5.8.0 CubeMX started to freeze on "Generating user code" step. When "keep user code while regenerating" option is disabled, the generation works fine, but it's a huge pain to merge user code by hand.

Any plans to fix this bug (or better - update CMSIS inside ST firmware packages, so that DSP and FPU work out-of-the-box on STM32F4), ST?

P.S. Same issue was reported back in February: https://community.st.com/s/question/0D53W00000beboI/strange-error-message-when-using-cmsis-57-with-stm-cubeide-during-code-generation-after-update-to-cubeide-160