STM32H74A3: How can I switch SPI Mode for 2 SPI-Slaves on the fly
I have a system with an STM32H74A3, which uses one SPI port for different slaves which use different SPI modes.
One Slave needs Mode 3 (Pol.High/2ndEdge) and 8 Bit Data size, the other needs Mode 0 (Pol.Low/1stEdge) and 16 Bit.
Clock Speed is the same for both SPIs.
Init Code for Mode 3:
HandleSpiBMP.Instance = SPI2;
HandleSpiBMP.Init.Mode = SPI_MODE_MASTER;
HandleSpiBMP.Init.Direction = SPI_DIRECTION_2LINES;
HandleSpiBMP.Init.DataSize = SPI_DATASIZE_8BIT;
HandleSpiBMP.Init.CLKPolarity = SPI_POLARITY_HIGH;
HandleSpiBMP.Init.CLKPhase = SPI_PHASE_2EDGE;
HandleSpiBMP.Init.NSS = SPI_NSS_SOFT;
HandleSpiBMP.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
HandleSpiBMP.Init.FirstBit = SPI_FIRSTBIT_MSB;
HandleSpiBMP.Init.TIMode = SPI_TIMODE_DISABLE;
HandleSpiBMP.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
HandleSpiBMP.Init.CRCPolynomial = 0x0;
HandleSpiBMP.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
HandleSpiBMP.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
HandleSpiBMP.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
HandleSpiBMP.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
HandleSpiBMP.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
HandleSpiBMP.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
HandleSpiBMP.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
HandleSpiBMP.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
HandleSpiBMP.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
HandleSpiBMP.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&HandleSpiBMP) != HAL_OK)
{
Error_Handler();
}
Init Code for Mode 0:
HandleSpiMurataIMU.Instance = SPI2;
HandleSpiMurataIMU.Init.Mode = SPI_MODE_MASTER;
HandleSpiMurataIMU.Init.Direction = SPI_DIRECTION_2LINES;
HandleSpiMurataIMU.Init.DataSize = SPI_DATASIZE_16BIT; // <<
HandleSpiMurataIMU.Init.CLKPolarity = SPI_POLARITY_LOW; // <<
HandleSpiMurataIMU.Init.CLKPhase = SPI_PHASE_1EDGE; // <<
HandleSpiMurataIMU.Init.NSS = SPI_NSS_SOFT;
HandleSpiMurataIMU.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
HandleSpiMurataIMU.Init.FirstBit = SPI_FIRSTBIT_MSB;
HandleSpiMurataIMU.Init.TIMode = SPI_TIMODE_DISABLE;
HandleSpiMurataIMU.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
HandleSpiMurataIMU.Init.CRCPolynomial = 0x0;
HandleSpiMurataIMU.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
HandleSpiMurataIMU.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
HandleSpiMurataIMU.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
HandleSpiMurataIMU.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
HandleSpiMurataIMU.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
HandleSpiMurataIMU.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
HandleSpiMurataIMU.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
HandleSpiMurataIMU.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
HandleSpiMurataIMU.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
HandleSpiMurataIMU.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&HandleSpiMurataIMU) != HAL_OK)
{
Error_Handler();
}
When setting up the system to use only the first setup with Mode 3, this SPI slave is working perfectly.
When I switch to Mode 0 to support the second slave, this one works too.
But as soon as I switch back to Mode 3 the first slave doesn't deliver correct values.
I call HAL_SPI_DeInit() before HAL_SPI_Init with the alternative setup.
Even a delay of 100 µsec after the new Init is called doesn't help.
Did anyone use this kind of SPI usage? How can I achieve to get this working with both slaves?
Thank you for any assistance.
GS