2023-11-30 4:12 PM
Hello,
The STM32U585 Reference Manual say these chips have one AES and one SAES peripheral. In turn each of these have an "AES core algorithm (AEA)" component. I expect that to mean that there are two physically independent AEA's on the chip. Is that correct?
Thanks
Solved! Go to Solution.
2023-11-30 5:52 PM
With the exception of the shared key interface from SAES -> AES, they are independent.
2023-11-30 5:52 PM
With the exception of the shared key interface from SAES -> AES, they are independent.