cancel
Showing results for 
Search instead for 
Did you mean: 

AES v SAES

EC.3
Associate III

Hello,

The STM32U585 Reference Manual say these chips have one AES and one SAES peripheral. In turn each of these have an "AES core algorithm (AEA)" component. I expect that to mean that there are two physically independent AEA's on the chip. Is that correct?

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

With the exception of the shared key interface from SAES -> AES, they are independent.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Guru

With the exception of the shared key interface from SAES -> AES, they are independent.

If you feel a post has answered your question, please click "Accept as Solution".